This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28032: Pls help to provide a example code for F28034 LFU

Part Number: TMS320F28032
Other Parts Discussed in Thread: C2000WARE

Dear Sir

Pls help to provide a example code for F28034 LFU .

  • Hello, 

    This device does not have an LFU example, you can refer to the flash kernel example for this device, which is located at C2000Ware_x_xx_xx_xx > device_support > f2803x > examples > c28 > f2803x_flash_kernel.

    The F28004x device has a LFU example, it is located at C2000Ware_x_xx_xx_xx > driverlib > f28004x > examples > flash, select flashapi_ex2_sci_kernel. 

    Please also refer to the flash kernel app note: www.ti.com/lit/sprabv4 

    Anu