This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28384D: MCBSP Transmits 3 leading 0 bits prior to set Tx values

Part Number: TMS320F28384D

I cannot find anything in the setup configuration to cause this. Any ideas?

  • David,

    I'm not aware of a reason this should be happening.  Would it be possible to share your setup/use code for me to look at?

    Best,

    Matthew

  • void InitMcbspb(void)
       {
       // McBSP-B register settings
    
       McbspbRegs.SPCR2.all=0x0000;     // Reset FS generator, sample rate generator & transmitter
       McbspbRegs.SPCR1.all=0x0000;     // Reset Receiver, Right justify word
       //Loopback mode does not apply here
       //McbspbRegs.SPCR1.bit.DLB = 1;  // Enable loopback mode for test. Comment out for normal McBSP transfer mode.
    
    
       McbspbRegs.MFFINT.all=0x0;           // Disable all interrupts
    
       McbspbRegs.RCR1.all=0x0;
       McbspbRegs.RCR2.all=0x0;         // Single-phase frame, No companding (Receive)
       McbspbRegs.RCR1.bit.RFRLEN1 = MCBSP_RECEIVE_FRAME_LENGTH(McBSPNumRxWords);
       McbspbRegs.RCR2.bit.RDATDLY = MCBSP_0_BIT_DELAY;
       //McbspbRegs.RCR2.bit.RFIG    = 1; //Ignore incoming frame-sync pulses (the FPGA only sends one for the whole packet)
    
       McbspbRegs.XCR1.all=0x0;
       McbspbRegs.XCR2.all=0x0;         // Single-phase frame, No companding (Transmit)
       McbspbRegs.XCR1.bit.XFRLEN1 = MCBSP_TRANSMIT_FRAME_LENGTH(McBSPNumTxWords);
       McbspbRegs.XCR2.bit.XDATDLY = MCBSP_0_BIT_DELAY;
    
       InitMcbspb16bit();         //Sets RCR1.bit.RWDLEN1 and XCR1.bit.XWDLEN1
    
       McbspbRegs.PCR.bit.FSXM     = MCBSP_INTERNAL_TX_FRAME_SYNC;       // FSX generated internally, FSR derived from an external source
       McbspbRegs.PCR.bit.CLKXM    = MCBSP_INTERNAL_TX_CLK;              // CLK-TX is driven by the sample rate generator clock
       McbspbRegs.PCR.bit.CLKRM    = MCBSP_INTERNAL_RX_CLK;              // CLK-RX is driven by the sample rate generator clock
       McbspbRegs.PCR.bit.CLKXP    = MCBSP_TX_DATA_UPDATE_ON_FALLING;    // TX data clocked on falling edges (should be sampled on rising)
       McbspbRegs.PCR.bit.CLKRP    = MCBSP_RX_SAMPLED_ON_FALLING;        // RX data sampled on falling edges
    
       //CLKSM=1 and SCLKME=0 defines the sample-rate-generator based on the internal sample rate generator
       McbspbRegs.PCR.bit.SCLKME   = 0;
       McbspbRegs.SRGR2.bit.CLKSM  = MCBSP_SAMPLE_RATE_GENERATOR_LSPCLK;
    
       McbspbRegs.SRGR2.bit.FPER   = MCBSP_FRAME_SYNC_PERIOD(16);        // FPER = 16 bits plus 1 FS bit
       McbspbRegs.SRGR1.bit.FWID   = MCBSP_FRAME_SYNC_PULSE_WIDTH(1);    // Frame Width = 1 CLKG period
       McbspbRegs.SRGR1.bit.CLKGDV = MCBSP_CLOCK_DIVIDE(McBSPClockDivider);// CLKG frequency = LSPCLK/(x) (or SYSCLKOUT/{x*4})
    
       //For debug: stop the McBSP clock on emulator halt:
       McbspbRegs.SPCR2.bit.FREE   = 0;                                  //Stop the clock on breakpoint halt
       McbspbRegs.SPCR2.bit.SOFT   = 0;                                  //And don't finish the word
    
       delay_loop();                    // Wait at least 2 SRG clock cycles
       McbspbRegs.SPCR2.bit.GRST=1;     // Enable the sample rate generator
       clkg_delay_loop();               // Wait at least 2 CLKG cycles
       McbspbRegs.SPCR2.bit.XRST=1;     // Release TX from Reset
       McbspbRegs.SPCR1.bit.RRST=1;     // Release RX from Reset
       McbspbRegs.SPCR2.bit.FRST=1;     // Frame Sync Generator reset
    
       //Connect DMA channel 5 to McBSPA receive:
       DMACH5AddrConfig((U16 *)&McBSPRxDataUInt[0], (U16*)&McbspbRegs.DRR1.all);
    
       EALLOW;
       //The inner-loop is the burst per trigger:
       DMA5_WRITE_BURST_SIZE(1);                    //One "DATASIZE" value at a time
       DMA5_WRITE_SRC_BURST_STEP(0);                //The transfer-loop will increment
       DMA5_WRITE_DST_BURST_STEP(0);                //All transmissions written to a single address (no increment)
    
       //The outer-loop transfers a total of BURST_SIZE * TRANSFER_SIZE words.
       DMA5_WRITE_TRANSFER_SIZE(McBSPNumRxWords);   //Number of transfers of 1 word(burst) at a time
       DMA5_WRITE_SRC_TRANSFER_STEP(0);             //Source address does not change
       DMA5_WRITE_DST_TRANSFER_STEP(1);             //1 word increment after each 1-word received
    
       DMA5_WRITE_SOURCE_WRAP_SIZE(0xFFFF);         // Wrap disabled
       DMA5_WRITE_SOURCE_WRAP_STEP(0xFFFF);         // Wrap disabled
       DMA5_WRITE_DST_WRAP_SIZE(0xFFFF);            // Wrap disabled
       DMA5_WRITE_DST_WRAP_STEP(0xFFFF);            // Wrap disabled
    
       // Set up MODE Register:
       DmaClaSrcSelRegs.DMACHSRCSEL2.bit.CH5 = DMA_MREVTB;   // Triggered by DMA_MREVTB
       DmaRegs.CH5.MODE.bit.PERINTSEL   = 5;                 // DMA channel 5
       DmaRegs.CH5.MODE.bit.CHINTE      = CHINT_DISABLE;     // No Transfer-complete interrupt
       DmaRegs.CH5.MODE.bit.DATASIZE    = SIXTEEN_BIT;       // 16-bit data size transfers
       DmaRegs.CH5.MODE.bit.CONTINUOUS  = CONT_DISABLE;      // Channel is disabled after transfer is complete
       DmaRegs.CH5.MODE.bit.ONESHOT     = ONESHOT_DISABLE;   // Oneshot disabled (One burst per event)
       DmaRegs.CH5.MODE.bit.CHINTMODE   = CHINT_END;         // Generate interrupt to CPU at end of transfer
       DmaRegs.CH5.MODE.bit.PERINTE     = PERINT_ENABLE;     // Peripheral interrupt enable
       DmaRegs.CH5.MODE.bit.OVRINTE     = OVERFLOW_DISABLE;  // Disable the overflow interrupt
    
       // Clear any spurious flags:
       DmaRegs.CH5.CONTROL.bit.PERINTCLR = 1;       // Clear any spurious interrupt flags
       DmaRegs.CH5.CONTROL.bit.ERRCLR    = 1;       // Clear any spurious sync error flags
    
       EDIS;
       StartDMACH5();                               //The transfer starts when the event/interrupt occurs:
       //When the McBSP receives a word, it generates the REVT events to the DMA-engine, which reads the word.
       //It is assumed the transfer is complete by the end of the HSL.
    
    
       //Connect DMA channel 6 to McBSPB transmit:
       DMACH6AddrConfig((U16*)&McbspbRegs.DXR1.all, (U16 *)&McBSPTxDataUInt[0]);
    
       EALLOW;
       //The inner-loop is the burst per trigger:
       DMA6_WRITE_BURST_SIZE(1);                    //One "DATASIZE" value at a time
       DMA6_WRITE_SRC_BURST_STEP(0);                //The transfer-loop will increment
       DMA6_WRITE_DST_BURST_STEP(0);                //All transmissions written to a single address (no increment)
    
       //The outer-loop transfers a total of BURST_SIZE * TRANSFER_SIZE words.
       DMA6_WRITE_TRANSFER_SIZE(McBSPNumTxWords);   //Number of transfers of 1 word(burst) at a time
       DMA6_WRITE_SRC_TRANSFER_STEP(1);             //1 word increment after each 1-word transmitted
       DMA6_WRITE_DST_TRANSFER_STEP(0);             //Destination address does not change
    
       DMA6_WRITE_SOURCE_WRAP_SIZE(0xFFFF);         // Wrap disabled
       DMA6_WRITE_SOURCE_WRAP_STEP(0xFFFF);         // Wrap disabled
       DMA6_WRITE_DST_WRAP_SIZE(0xFFFF);            // Wrap disabled
       DMA6_WRITE_DST_WRAP_STEP(0xFFFF);            // Wrap disabled
    
       // Set up MODE Register:
       DmaClaSrcSelRegs.DMACHSRCSEL2.bit.CH6 = DMA_MXEVTB;   // Triggered by DMA_MXEVTB
       DmaRegs.CH6.MODE.bit.PERINTSEL   = 6;                 // DMA channel 6
       DmaRegs.CH6.MODE.bit.CHINTE      = CHINT_DISABLE;     // No Transfer-complete interrupt
       DmaRegs.CH6.MODE.bit.DATASIZE    = SIXTEEN_BIT;       // 16-bit data size transfers
       DmaRegs.CH6.MODE.bit.CONTINUOUS  = CONT_DISABLE;      // Channel is disabled after transfer is complete
       DmaRegs.CH6.MODE.bit.ONESHOT     = ONESHOT_DISABLE;   // Oneshot disabled (One burst per event)
       DmaRegs.CH6.MODE.bit.CHINTMODE   = CHINT_END;         // Generate interrupt to CPU at end of transfer
       DmaRegs.CH6.MODE.bit.PERINTE     = PERINT_ENABLE;     // Peripheral interrupt enable
       DmaRegs.CH6.MODE.bit.OVRINTE     = OVERFLOW_DISABLE;  // Disable the overflow interrupt
    
       // Clear any spurious flags:
       DmaRegs.CH6.CONTROL.bit.PERINTCLR = 1;       // Clear any spurious interrupt flags
       DmaRegs.CH6.CONTROL.bit.ERRCLR    = 1;       // Clear any spurious sync error flags
    
       EDIS;
       StartDMACH6();                               //The transfer starts when the event/interrupt occurs:
       //Force an event (trigger) onto the DMA engine by calling DMA6_FORCE_TRIGGER(), which inserts an event into DMA6. Then
       //the McBSP transmit-register is written with the first array element. The McBSP produces an XEVT when XRDY is true,
       //which kicks off the next word-write. It is assumed the transfer is complete by the end of the HSL.
       }
    

  • David,

    I'll reply back tomorrow in out of the office today with limited access to my PC/EVM.

    Best,

    Matthew 

  • David,

    Could you try and write directly to the McbspaRegs.DXR1 register from the CPU vs using the DMA and note if the behavior is different?  I'd like to see if the DMA is somehow in play here.

    Best,

    Matthew