Part Number: TMS320F28035
Other Parts Discussed in Thread: UNIFLASH, LAUNCHXL-F280049C, TMDSCNCD28035, , TMDSCNCD28035ISO, TIDM-BUCKBOOST-BIDIR, C2000WARE, LAUNCHXL-F280025C, TMDSEMU200-U, TMDSEMU110-U
Hi Team,
I have procured one TIDU638 board and C200 Microcontroller (TMS320F28035PNT) and as per the instruction I have made all the necessary connection (hardware Prospect) i.e.
1. Make sure nothing is connected to the board, and no power is being supplied to the board.
2. Insert the controlCARD into the controlCARD connector if it is not already installed (F28035 ISO DIMM
CARD).
3. Set the following switch settings on the controlCARD:
• Control Card SW3 is in the ON position (JTAG Connection)
• Control Card SW2, Position 1 = ON, Position 2 = ON
4. Connect a DC load between VOPWR and VORTN (make sure the output load is of the appropriate
value needed for the test).
5. Connect a USB cable (mini-to-A cable) from the control card to the host computer. LD4 on the control
card will light up to indicate a successful USB connection.
6. Make sure the following jumpers are connected or disconnected:
(a) LK201: Connected (enables on-board bias power)
(i) If desired to supply 5 V and 12 V externally, then leave this jumper open, and supply 5 V and
12 V externally to their test points.
(b) LOOP STIM: Leave the jumper open.
(c) LK202, LK203: Connect jumpers horizontally at 5- and 12-V labels.
(i) If 5 V and 12 V are supplied externally, leave these jumpers open.
(d) LK301, LK302: Connect jumpers vertically for normal configuration.
I have tried both external powering the board and proving 12v & 5V externally. While trying to flash the code on to the control card using CCS or Uniflash using JTAG connector and LAUNCHXL-F280049C the controller is not getting detected.
If you can please suggest me how to resolve the issue.