Other Parts Discussed in Thread: C2000WARE
Hi all,
I copied the example project found here: C:\ti\c2000\C2000Ware_4_01_00_00\device_support\f2837xd\examples\dual\flash_programming\cpu01 to a new workspace. To do this, I imported the example project to my workspace, but it contained all linked files. Since I wanted to modify the source files without altering the originals, I exported the project using the "Resolve and export linked resources" option. After importing the exported project into a my workspace, I included some libraries and source files that were missing.
However, now I am getting the strange warning shown in the screenshot. The original example project compiled without any problems. I'm not sure why mine doesn't.

Thanks,
- Matthew