Part Number: TMS320F280049C
Hi:
is there documentation that is available that identifies how the CAN bit timing is identified in BTR0, BTR1 registers.
Im doing the following:
CAN CLK = 100Mhz
CAN Baud rate: 1Mbaud
TSEG1: 3
TSEG2: 1
SJW: 1
BRP: 20
sample point of 80%.
I just need to know how to convert this into the BTR0/1 registers.
Appreciate the help,
Abe