Part Number: TMS320F28035
Other Parts Discussed in Thread: UNIFLASH
Dear Champs,
I am asking this for our customer.
The user used to use C2000-GANG.
But because there is something wrong with C2000-GANG now (it's being dealt with), the user asked TI to have a backup solution using XDS110 + Uniflash.
The user uses CSM.
In the production line, it's required to update code (that is, the image on F28035 is already with CSM) sometimes.
In C2000-GANG, the user needs only to setup a correct CSM password for the first time on its GUI and it can be used to update FW code even if there is already a secured image.
Can Uniflash be used in this way?
That is, to setup a correct CSM password for the first time and then use it to program C2000 device with one click no matter its flash is empty or already with a secured image?
If yes, would you please show us how to do it?
If not, would you please add this function?
Wayne Huang