Part Number: TMS320F28379D
Hi,
I am trying the SCI echoback example on the 28379D control card. The example works well when I connect to GPIO28,29 using Putty terminal and configuring the COMM to the XDS serial port to which the debugger is connected. I tried to use a separate USB to serial DB9 adapter however that seems to be loading garbage data to the terminal window. I tried two things:
1) Tried connecting to the pins GPIO28 29 on the experimenters kit pinout through the DB9 connector and configuring the COMM to the new Comm port
2) Tried changing the serial comm channel to sci-b and changed the pinouts and connected through the DB9 connector again. This was also downloading the same garbage data.
Is it not possible to connect to the board through a separate USB to serial adapter? or is any additional configuration needed?
Thanks a lot,
Aditya