This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280025C: Using API's in CCS12 with "auto complete"

Part Number: TMS320F280025C
Other Parts Discussed in Thread: C2000WARE

I am used to the method of working with hardware such as is done with the 28069. If I want to manipulate the serial port, I start typing "SciaRegs.SCIFFTX...etc". As I type, the posssible options are available to see. With the 280025, I can not find the correct files that would allow me to reference the hardware in a similar fashio. Rather, there are now "API's" that we are being encouraged touse.

Problem is they take longer to look up and then as I am typing, therre is no auto complete to aid in finding the various parameters the API expects. So, questions:

1. Is there a file and correct settings so I can program the 280025 the same way I do on he 28069?

2. OR, can "auto complete" or something like that be enabled so the "API's" are easier to use?

Thanks, 

David