This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F241 On-chip Flash Programming Using XDS510PP Emulator

Our old test system was using Windows98 to flash program the TMS320F241 on board device but it quit working so we are trying to move the programming over to an XP station but with the existing flash programming commands, it keeps encountering a PRG2XXPP.EXE problem. Then when it gets through this, during the emurstpp.exe portion, it comes back and says that there is no communications or the POD has no power. We are powering it up seperately. When it is checked using SDconfig it shows the pod is working (the red LED flashes) and the JTAG says that there is a device available. The documentation we have is dated 09/22/97 and is called TMX320F240 JTAG Based Flash Programmer. Is there anything newer and where is it located?