Part Number: TMS320F280025C
Hi Champ,
I am asking for my customer, while I am also not clear about this part.
What my customer want to do is they could do the offline firmware update(PSU no 12V voltage) with their end customer's system by receiving new image (firmware) through I2C.
Does the customer's need do with the serial flash programming ? If yes, what are the boot mode setting for using I2C ?
The process of firmware update we are thinking is when the device is power on, then the boot mode is selected to boot to flash, which it would jump to the flash entry point (0x80000), so the customer's bootloader is put over the place to decide whether to do the firmware update. After finished that, then jump to customer's application code. Is our concept correct ?
Would the expert kindly clarify more detailly about firmware update as my customer's want ?
We have tried to read related app notes, while we are still confused how to implement.
Thanks and regards,
Johnny.