Part Number: TMS320F28379D
Other Parts Discussed in Thread: C2000WARE
Hi Team,
Here're some issues from the customer may need your help:
I use an oscilloscope to test the SPI communication timing. The SPIA self-receiving and self-transmitting, the SPIA master and the SPIB slave are respectively tested.
The CCS debug interface displays normally during the SPIA self-receiving and self-testing. The oscilloscope measures SCLK as shown in the figure below, 8 pulses are in a group, and the width of a single pulse is 12.4us (both high and low level time are 6.2us), but there will be a time interval of 31.4us between each group of pulses. Is this normal?

Measured the SIMO pin and found that it will continue to send the same data. The measurement time is about 32.3ms, and the data is repeated about 243 times. How to solve this?

The following is the program of SPIA self-receiving and self-sending:
/*
* SPI self-receive and self-transmit
*
*/
#include "F28x_Project.h"
typedef unsigned char Uint8;
//statement
void gpio_init(); //Configure all GPIO ports connected to the PCB board (including 3-wire SPI)
void spia_init();
void spia_xmit(Uint8 a);
//global variable
char sdata;
char rdata;
void main()
{
//initialization
InitSysCtrl();
InitGpio();
DINT;//disable interrupt
InitPieCtrl();
IER = 0x0000;
IFR = 0x0000;
InitPieVectTable();
gpio_init();
spia_init();
sdata = 0x0045;
for(;;)
{
spia_xmit(sdata);
while(SpiaRegs.SPISTS.bit.INT_FLAG != 1){}
rdata = SpiaRegs.SPIRXBUF;
sdata++;
}
}
void gpio_init()
{
/*
* 60 SPICLKA_DA SPIA CLK
* 59 SPISOMIA_DA SPIA SOMI
* 58 SPISIMOA_DA SPIA SIMO
*/
EALLOW;
//SPI
//DA(enable、asynchronous、SPI)
GpioCtrlRegs.GPBPUD.bit.GPIO60 = 0;
GpioCtrlRegs.GPBQSEL2.bit.GPIO60 = 3;
GpioCtrlRegs.GPBMUX2.bit.GPIO60 = 3;
GpioCtrlRegs.GPBGMUX2.bit.GPIO60 = 3;//SPICLKA
GpioCtrlRegs.GPBPUD.bit.GPIO59 = 0;
GpioCtrlRegs.GPBQSEL2.bit.GPIO59 = 3;
GpioCtrlRegs.GPBMUX2.bit.GPIO59 = 3;
GpioCtrlRegs.GPBGMUX2.bit.GPIO59 = 3;//SPISOMIA
GpioCtrlRegs.GPBPUD.bit.GPIO58 = 0;
GpioCtrlRegs.GPBQSEL2.bit.GPIO58 = 3;
GpioCtrlRegs.GPBMUX2.bit.GPIO58 = 3;
GpioCtrlRegs.GPBGMUX2.bit.GPIO58 = 3;//SPISIMOA
EDIS;
}
void spia_init()
{
//DAC1282 clock polarity(CPOL)is 0,clock phase(CPHA)is 0
//Configuration Control Register(8 bits reserved,0000 0000 0000 0111 = 0x0007)
SpiaRegs.SPICCR.bit.SPISWRESET = 0;//SPI reset
SpiaRegs.SPICCR.bit.CLKPOLARITY = 0;//clock polarity is 0(SCK idle is low)
SpiaRegs.SPICCR.bit.HS_MODE = 0;//Turn off high speed mode
SpiaRegs.SPICCR.bit.SPILBK = 1;//Turn off loopback mode
SpiaRegs.SPICCR.bit.SPICHAR = (8-1);//Word length 8 bits
//运行控制寄存器(11位保留,0000 0000 0000 0110 = 0x0006)
SpiaRegs.SPICTL.bit.OVERRUNINTENA = 1;//Disable receive overflow interrupt
SpiaRegs.SPICTL.bit.CLK_PHASE = 0;//clock phase is 0(Sampled on the first transition edge)
SpiaRegs.SPICTL.bit.MASTER_SLAVE = 1;//MCU master
SpiaRegs.SPICTL.bit.TALK = 1;//enable master transmit
SpiaRegs.SPICTL.bit.SPIINTENA = 0;//disable SPI interrupt
//SpiaRegs.SPISTS.all = 0;
//baud rate register(9 bits reserved,0000 0000 0000 007C)
/*
* LSPCLKfreq=CPUfreq/n //(n=1,2,4,6,8,10,12,14)
* SPI Baud Rate=LSPCLKfreq/(SPIBRR+1)
* without adding an external auxiliary clock
* The CPU frequency of F28379D is 10MHz, the corresponding minimum low-speed peripheral clock is 715KHz, and the minimum baud rate is 5586SPS
* This minimum baud rate is greater than the maximum baud rate 4000SPS when FIR filter mode is selected
* Therefore, the Sinc filter mode is selected, the baud rate is set to 8000SPS, and the frequency is divided by 10,SPIBRR=124=0x007C
*/
EALLOW;
ClkCfgRegs.LOSPCP.all = 0x0005;//101(divide by 10)
EDIS;
SpiaRegs.SPIBRR.bit.SPI_BIT_RATE = 0x007C;
//Priority Control Register
SpiaRegs.SPIPRI.bit.FREE = 1;//Free run during simulation, pause on breakpoint does not stop SPI
//Stop SPI software reset ready to receive or transmit
SpiaRegs.SPICCR.bit.SPISWRESET = 1;
}
void spia_xmit(Uint8 a)
{
SpiaRegs.SPITXBUF = a;//Pass 8-bit data to serial transmit buffer
}
Connection for SPIA master SPIB slave test:
SPIA CLK-SPIB CLK
SPIA SIMO-SPIB SOMI
SPIA SOMI-SPIB SIMO
The SCLK waveform is the same as that of SPIA, but after a period of normal operation, the debug interface shows that rdata is always FFFF, SpiaRegs.SPITS.bit.INT_FLAG is always 1, and the while loop cannot be jumped out. How should this be resolved?

Program for SPIA master and SPIB slave:
/*
*
*
*/
#include "F28x_Project.h"
typedef unsigned char Uint8;
void gpio_init();
void spia_init();
void spia_xmit(Uint8 a);
void spib_init();
void spib_xmit(Uint8 a);
char sdata;
char rdata;
int i;
void main()
{
InitSysCtrl();
InitGpio();//GPIO
DINT;
InitPieCtrl();
IER = 0x0000;
IFR = 0x0000;
InitPieVectTable();
gpio_init();
spia_init();
spib_init();
sdata = 0x0000;
rdata = 0x0000;
for(;;)
{
spia_xmit(sdata);
while(SpibRegs.SPISTS.bit.INT_FLAG != 1){}
rdata = SpibRegs.SPIRXBUF;
sdata++;
}
}
void gpio_init()
{
/*
* 60 SPICLKA_DA SPIA CLK
* 59 SPISOMIA_DA SPIA SOMI
* 58 SPISIMOA_DA SPIA SIMO
*
* 65 SPICLKB_AD SPIB CLK
* 64 SPISOMIB_AD SPIB SOMI
* 63 SPISIMOB_AD SPIB SIMO
*/
EALLOW;
//SPI
//DA
GpioCtrlRegs.GPBPUD.bit.GPIO60 = 0;
GpioCtrlRegs.GPBQSEL2.bit.GPIO60 = 3;
GpioCtrlRegs.GPBMUX2.bit.GPIO60 = 3;
GpioCtrlRegs.GPBGMUX2.bit.GPIO60 = 3;//SPICLKA
GpioCtrlRegs.GPBPUD.bit.GPIO59 = 0;
GpioCtrlRegs.GPBQSEL2.bit.GPIO59 = 3;
GpioCtrlRegs.GPBMUX2.bit.GPIO59 = 3;
GpioCtrlRegs.GPBGMUX2.bit.GPIO59 = 3;//SPISOMIA
GpioCtrlRegs.GPBPUD.bit.GPIO58 = 0;
GpioCtrlRegs.GPBQSEL2.bit.GPIO58 = 3;
GpioCtrlRegs.GPBMUX2.bit.GPIO58 = 3;
GpioCtrlRegs.GPBGMUX2.bit.GPIO58 = 3;//SPISIMOA
//SPI
//DA
GpioCtrlRegs.GPCPUD.bit.GPIO65 = 0;
GpioCtrlRegs.GPCQSEL1.bit.GPIO65 = 3;
GpioCtrlRegs.GPCMUX1.bit.GPIO65 = 3;
GpioCtrlRegs.GPCGMUX1.bit.GPIO65 = 3;//SPICLKB
GpioCtrlRegs.GPCPUD.bit.GPIO64 = 0;
GpioCtrlRegs.GPCQSEL1.bit.GPIO64 = 3;
GpioCtrlRegs.GPCMUX1.bit.GPIO64 = 3;
GpioCtrlRegs.GPCGMUX1.bit.GPIO64 = 3;//SPISOMIB
GpioCtrlRegs.GPBPUD.bit.GPIO63 = 0;
GpioCtrlRegs.GPBQSEL2.bit.GPIO63 = 3;
GpioCtrlRegs.GPBMUX2.bit.GPIO63 = 3;
GpioCtrlRegs.GPBGMUX2.bit.GPIO63 = 3;//SPISIMOB
EDIS;
}
void spia_init()
{
SpiaRegs.SPICCR.bit.SPISWRESET = 0;
SpiaRegs.SPICCR.bit.CLKPOLARITY = 0;
SpiaRegs.SPICCR.bit.HS_MODE = 0;
SpiaRegs.SPICCR.bit.SPILBK = 1;
SpiaRegs.SPICCR.bit.SPICHAR = (8-1);
SpiaRegs.SPICTL.bit.OVERRUNINTENA = 1;
SpiaRegs.SPICTL.bit.CLK_PHASE = 0;
SpiaRegs.SPICTL.bit.MASTER_SLAVE = 1;//MCU master
SpiaRegs.SPICTL.bit.TALK = 1;
SpiaRegs.SPICTL.bit.SPIINTENA = 0;
//SpiaRegs.SPISTS.all = 0;
/*
* LSPCLKfreq=CPUfreq/n //(n=1,2,4,6,8,10,12,14)
* SPI Baud Rate=LSPCLKfreq/(SPIBRR+1)
*
*
*
*
*/
EALLOW;
ClkCfgRegs.LOSPCP.all = 0x0005;//101
EDIS;
SpiaRegs.SPIBRR.bit.SPI_BIT_RATE = 0x007C;
SpiaRegs.SPIPRI.bit.FREE = 1;
SpiaRegs.SPICCR.bit.SPISWRESET = 1;
}
void spib_init()
{
SpibRegs.SPICCR.bit.SPISWRESET = 0;
SpibRegs.SPICCR.bit.CLKPOLARITY = 0;
SpibRegs.SPICCR.bit.HS_MODE = 0;
SpibRegs.SPICCR.bit.SPILBK = 1;
SpibRegs.SPICCR.bit.SPICHAR = (8-1);
SpibRegs.SPICTL.bit.OVERRUNINTENA = 1;
SpibRegs.SPICTL.bit.CLK_PHASE = 0;
SpibRegs.SPICTL.bit.MASTER_SLAVE = 0;//MCU master
SpibRegs.SPICTL.bit.TALK = 1;
SpibRegs.SPICTL.bit.SPIINTENA = 0;
//SpiaRegs.SPISTS.all = 0;
/*
* LSPCLKfreq=CPUfreq/n //(n=1,2,4,6,8,10,12,14)
* SPI Baud Rate=LSPCLKfreq/(SPIBRR+1)
*
*
*
*
*/
EALLOW;
ClkCfgRegs.LOSPCP.all = 0x0005;//101
EDIS;
SpibRegs.SPIBRR.bit.SPI_BIT_RATE = 0x007C;
SpibRegs.SPIPRI.bit.FREE = 1;
SpibRegs.SPICCR.bit.SPISWRESET = 1;
}
void spia_xmit(Uint8 a)
{
SpiaRegs.SPITXBUF = a;
}
Thanks & Regards
Yale Li