This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28069M: gmake error while compile the instaSpin Project

Part Number: TMS320F28069M

Hello Dear,

I am using micro controller TMS320f28069M and CCS V11 for Instaspin Motion control.

While build the projects of Instaspin's Labs I have gmake file errors.

I already tried

1) Re install CCS

2)change compiler Versions

3) Change the runtime support library

Help me to get over this errors.

For reference of error files are attached.

Thank You

  • You may try to just import the example lab within CCS without any changes, to see what happen? And did you have the same issue on the other labs?

    Under "Runtime support library" in "Properties of Project", you need to select "rts2800_ml.lib". Don't need to select the device and core, just keep using "Generic C28xx device" by default.

  • I try  import the example lab only without any changes, and I faced same issue. I don't have any error with other labs example.

    and with selection of "generic c28xx devices" I don't have any errors.

    But I am using "TMS320C2000 Development tool" ,Is it fine to use "generic c28xx devices" ?

  • Thank you luo, It's solved. It's encoder only.the encoder is missing some pulses because of alignment issue.

    But the inertia test with lab 12a at rated speed it's still give error 2004.