Part Number: TMS320F28388D
Other Parts Discussed in Thread: C2000WARE
Hello:
Why does the SPI configure all pins to pull up when configuring SPI pin parameters?
Does the pull up here make sense? I have tried to configure the clock pin and MOSI pin as push-pull ,then, the MISO pin as floating air input, and the SPI also works fine
thanks
path:
C:\ti\c2000\C2000Ware_3_03_00_00\driverlib\f2838x\examples\c28x\spi
“spi_ex6_eeprom “,and “spi_ex5_external_loopback”
// GPIO16 is the SPISIMOA pin.
//
GPIO_setMasterCore(16, GPIO_CORE_CPU1);
GPIO_setPinConfig(GPIO_16_SPIA_SIMO);
GPIO_setPadConfig(16, GPIO_PIN_TYPE_PULLUP);
GPIO_setQualificationMode(16, GPIO_QUAL_ASYNC);
//
// GPIO17 is the SPISOMIA.
//
GPIO_setMasterCore(17, GPIO_CORE_CPU1);
GPIO_setPinConfig(GPIO_17_SPIA_SOMI);
GPIO_setPadConfig(17, GPIO_PIN_TYPE_PULLUP);
GPIO_setQualificationMode(17, GPIO_QUAL_ASYNC);
//
// GPIO18 is the SPICLKA.
//
GPIO_setMasterCore(18, GPIO_CORE_CPU1);
GPIO_setPinConfig(GPIO_18_SPIA_CLK);
GPIO_setPadConfig(18, GPIO_PIN_TYPE_PULLUP);