Part Number: TMS320F28386S
HI,
I am using the SPI to Write and Read Data from an external Gyro.
I am using the DMA to save CPU time writing and reading from the SPI FIFO.
After the data is received, some processing needs to be done on the received data.
I want to do this processing on the CLA.
I based my configuration on the "spi_ex5_loopback_dma" sample project.
I can confirm that data is send and received from the gyro when working on CPU1 memory.
To have the DMA write the received data from the spi directly to a memory with CLA access, I placed the rData Buffer within the "cla_chared" data section.
```
#pragma SET_DATA_SECTION("cla_shared")
volatile uint16_t rData[16]; // Gyro receive data buffer
#pragma SET_DATA_SECTION() // Reset section to default
```
However, It seems that the the data is not copied to the buffer.
The values at the buffer when the CLA task run is all 0's.
Am I doing something wrong?
Or maybe the DMA can't wright to memory that the CLA can access?
I attached the relevant2838x_FLASH_CLA_lnk_cpu1.rar linker command file.