Part Number: TMS320F28377D
Other Parts Discussed in Thread: SYSCONFIG,
Hi,
I want the EPWM5A to get output on GPIO Pin 100 in DSP.
HOW TO DO THIS???
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F28377D
Other Parts Discussed in Thread: SYSCONFIG,
Hi,
I want the EPWM5A to get output on GPIO Pin 100 in DSP.
HOW TO DO THIS???
Hi Vishal,
Which package variant are you using? For the 100-pin package, there are no pins with EPWM5, and for the 176-pin package, EPWM5A is only available on GPIO8 (pin 18). The 337-package uses ball numbers. So you would not be able to output EPWM5A to pin 100 since it is not muxed to that pin. I recommend using the TI PinMux tool (in SysConfig) to see what signals are available for which pins

Regards,
Peter
Can output bar logic or any other way by which I can take out the PWM other then the Muxed pons
Hi Vishal,
You can use the CLB module to pass signals out to a GPIO using an output xbar, however there is no output xbar muxed to pin 100 on any of our packages for TMS320F28377D. Typically you would input the EPWM signal into the CLB and then directly route it out through CLB outputs 4 or 5 to an output xbar.
Regards,
Peter