Part Number: TMS320F28069M
Hello Dear,
I am using micro controller TMS320f28069M and CCS V11 for Instaspin Motion control.
I have setup of PMSM Motor(Rated - 200 Hz,3000 rpm, 1.1A, 3phase 75 V) With US DIgital's Encoder E5-5000. This setup is Drive with,TMS320C2000.
With Lab12a I am getting error 2004. I try to go with minimum speed and max torque with decreasing "VelIdTorqueRampTime_sec" Variable .
but I have still 2004 Error and the motor is not spinning. here I attached two image one with error 2004 and an other one is Motor User Parameter.
I try lab 5 and it's working fine and the encoder is also working fine.
Now, What should I do to remove my error 2004.