Part Number: TMS320F28335
Other Parts Discussed in Thread: UNIFLASH
Dear Champs,
I am asking this for our customer.
Because there is something wrong with flash programming in the user's production line, the user wants to ensure every setting in our Uniflash is right.
In Uniflash Settings and Utilities,
1) What is below setting "clock configuration" used for? If the user uses a 20-MHz external crystal, should the user set below as 20 x 10 / 2 = 100 MHz?
As F28335 can run up to 150 MHz, but PLLCR max is 10 here.
How do we use the below settings to get 150 MHz?

2) What is below "Frequency Test" for?