Part Number: TMS320F280049C
Other Parts Discussed in Thread: UNIFLASH
Hello,
I have a new design with a TMS320F280049C.
The software runs correctly with debugger in CCS.
The software runs correctly if I flash the MCU with UniFlash tool, with the "Run Target After Program Load/Flash Operation" option enabled.
But if I reset the target (new power on), the MCU doesn't boot.
GPIO24 and GPIO32 have a 57K pull up.
With UniFlash, I can read at 0x0005F008 (Z1-OTP-BOOTPIN-CONFIG for standalone) = 0xFFFF FFFF.
Why doesn't the C2000 automatically run the software at reset ?
Thanks,
Nicolas