Other Parts Discussed in Thread: TMS320F28035
My application is a resonant DCDC converter. I'm using "just in time" adc sampling with CLA TMS320F28035.
The CLA task should always start in the middle of the EPWM3A on time, but when the circuit is powered, sometimes it works as expected and after some POWER ON / POWER OFF cycles the The start of CLA task is shifted to right (instead of start in the middle of the EPWM3A "ON TIME", it starts in the end of the EPWM3A "ON TIME").
someone has experienced that behaviour?
some idea to solve that issue?
Thanks in advance,
Ricardo
see waveforms in the end of this post
system description (main code lines for reference):
--------------------------------------------------------------------------------------
EPWM3A - Half-Bridge High-Side PWM signal
EPWM3B - Half-Bridge Low-Side PWM signal
ADCINA3 - OUTPUT VOLTAGE SAMPLE
AdcRegs.ADCSOC1CTL.bit.TRIGSEL = 0x9; // ADCS0CA event connected to ePWM3A
AdcRegs.ADCSOC1CTL.bit.CHSEL = 3; // ADCINA3 selected to SOC1
The PWM register are loaded according to the following:
EPwm3Regs.TBPRD= prd
EPwm3Regs.CMPA.half.CMPA = prd / 2
EPwm3Regs.CMPB = prd / 4
EPwm3Regs.ETSEL.bit.SOCASEL = ET_CTRU_CMPB; // SOCA on counter equal to CMPB when the timer is incrementing.
EPwm3Regs.ETSEL.bit.SOCAEN = 1; // Enable SOC on A group
EPwm3Regs.ETPS.bit.SOCAPRD = ET_1ST; // Trigger on every event
SOCA is trigged by EPWM3 When CMPB is equal to TBPRD / 4 which results in the start of conversion in the midle of the ON time of the switch connected to EPWM3A
-------------------------------------------------------------------------------------------------------------------------------
AdcRegs.ADCCTL1.bit.INTPULSEPOS = 0; // INT pulse generation occurs when ADC begins conversion
AdcRegs.INTSEL1N2.bit.INT1CONT = 1; // ADCINTx pulses are generated whenever an EOC pulse is generated irrespective if the
// flag bit is cleared or not.
AdcRegs.INTSEL1N2.bit.INT1SEL = 0x01; // EOC1 is trigger for ADCINTx
AdcRegs.INTSEL1N2.bit.INT1E = 1; // ADCINTx is enabled
ADCINA3 (SOC1) is configured to send EOC Early Interrupt Pulse in order to trigger CLA task 1
------------------------------------------------------------------------------------------------------------------------------
Cla1Regs.MPISRCSEL1.bit.PERINT1SEL = CLA_INT1_ADCINT1;
CLA task 1 is responsible for :
- READ ADCRESULT
- CONTROL LAW 2P2Z
- PWM REGISTER UPDATE
---------------------------------------------------------------------------------------------------------------------------------
in order to check the moment when CLA task 1 starts comparator 2 is being used to clear (0) pin 61
in order to check the moment when CLA task 1 stops comparator 2 is being used to set (1) pin 61
using the resource described above is possible to check the EPWM3 signals the BEGIN and the END of CLA task 1
------------------------------------------------------------------------------------------------------------------------------
yellow waveform (falling edge) - begining of CLA task
yellow waveform (low level) - CLA task execution time
yellow waveform (rising edge) - end of CLA task
pink waveform - EPWM3A
blue waveform - EPWM3B
----------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------
the waveform below shows the correct operation, the start of CLA task is alligned in the middle of EPWM3A (High Level)
----------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------
the waveform below shows the wrong operation, the start of CLA task is shifted to right insted of being alligned in the middle of EPWM3A (High Level)