Other Parts Discussed in Thread: TMS320F28335, TMS320F2812
I'm migrating from DSP TMS320F2812 fixed point to TMS320F28335 floating point.
But, after some analisys I realize that there is no significant difference in performance.
time for a multiplication: 128ns in floating point
while the fixed point takes about 117ns.
The project is already configured to run floating point
with the appropriate libraries and run from flash memory.
Is this performance normal?
Is there a specific library that I need to use to improve the DSP performance other than:
- rts2800_fp32.lib
- rts2800_fp32_fast_supplement.lib
#include <stdlib.h>
#include <stdio.h>
#include <math.h>
#include "DSP28x_Project.h"