This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSACDCKIT test data

Other Parts Discussed in Thread: CONTROLSUITE

 

Hi All,

Do TI have test data of TMDSACDCKIT such as efficiency, ripply noise etc on both PFC and full bridge converter?

Thanks,

NT

  • Hi,

    No we don't because this kit is a low voltage low power kit that does not completely represent the power stages in a typical application. The intention of this kit is not to show the best power stage design but to provide a learning platform to the user at a safe voltage and power level. This kit demonstrates how a C2000 device can interface to and control an ACDC system, and implement not just the control tasks but also supervisory and communication functions.

    Please also take a look at some of our full voltage high power kits. These kits are designed to closely represent power stages that are found in typical applications and also provide similar or better performance. These kits come with complete software, documentation and hardware package that is free to download as part of controlSuiteTM. You might be interested in our latest bridgeless PFC kit (TMDSHVBLPFCKIT) (85Vac -265Vac input, 390Vdc output, 300W) and the phase shifted full bridge kit (TMDSHVPSFBKIT) (380 - 400Vdc input, 12Vdc output, 600W). You can find more information on these and other kits at www.ti.com/c2000tools

    I hope this helps.

    Hrishi