Other Parts Discussed in Thread: TMS320F28027
Hello
I am trying to connect an XDS100v2 debugger to a board with a piccolo on and when I try to connect to the target i get the following error message
"C28xx: Error connecting to the target: (Error -1041 @ 0x0) The emulator reported an error. Confirm emulator configuration and connections, reset the emulator, and retry the operation. (Release 5.0.333.0)"
There was a similar post about this error and it was suggested to either run the dbgjtag.exe utility or re-install ccs. After running the dbgjtag.exe i got the following messages
"The test for the JTAG IR instruction path-length failed"
"The JTAG IR instruction scan-path is stuck-at-zero"
"The test for the JTAG DR bypass path-length failed"
"The JTAG DR bypass scan-path is stuck-at-zero"
So I am now wondering what to do... I am sure the XDS100 drivers are installed correctly since I can see the XDS100 Channel A and B in the device manager.
Any ideas?
Thanks