Hallo,
I'm a little bit confused regarding the GPIOs participating in the Boot-Mode selection process.
in the Datasheets (of 2803x and 2806x) only 2 GPIOs are mentioned - TDO and GPIO34
on the other hand in the "Hardware design guidelines" (SPRAAS1A), the GPIOs mentioned are: GPIO18,GPIO29,GPIO34 (so the TDO is NOT mentioned)
can you please clarify how the boot-mode process is executed, which GPIOs are considered, and what are your recommendations for applications requiring the boot-mode:
1. Flash
2. SCI
thanks a lot
Ari.