Part Number: TMS320F280025C
Other Parts Discussed in Thread: C2000WARE
Hi,
I have a problem I would like to change the interrupt priorities, so I have included the corresponding header file in my project. You will find the details here. The interrupts work well independently (I commented them and then reactivated them one by one in the main) but when I activate at least two of them it does not work anymore. For example when I activate the ADC interrupt and slow tasks I don't go to the ADC interrupt anymore.
I have looked at the examples but I can't find the solution.
Here a part of my main code /** * Interrupt for state machine sequencing and synchronization for slow background tasks all of 10ms. */ timer_cpu_config(CPUTIMER0_BASE, DEVICE_SYSCLK_FREQ, 10000); Interrupt_register(INT_TIMER0, &isr_slow_tasks); CPUTimer_enableInterrupt(CPUTIMER0_BASE); Interrupt_enable(INT_TIMER0); /** * Set up the ADC / ePWM SOC and initialize the end of conversion. * Enable interrupt. */ Interrupt_register(INT_ADCA1, &isr_adca); adc_config(ADCA_BASE); adc_config(ADCC_BASE); adc_init_soc(); Interrupt_enable(INT_ADCA1); /** * Enable Global Interrupt (INTM) and realtime interrupt (DBGM) */ EINT; ERTM;
__interrupt void isr_adca(void)
{
GPIO_writePin(4, 1); // for test
/// Save IER register on stack
volatile uint16_t tempPIEIER = HWREGH(PIECTRL_BASE + PIE_O_IER1);
/// See prioritized_isr_levels.h file for explanations and details. Set global priority with INTxPL values and others Gx_xPL
/// Set the global and group priority to allow CPU interrupts with higher priority.
/// The user must set the appropriate priority level for each of the CPU interrupts.
/// This is termed as the "global" priority. The priority level must be a number between 1 (highest) to 16 (lowest).
/// A value of 0 must be entered for reserved interrupts or interrupts that are not used.
IER |= M_INT1;
IER &= MINT1;
HWREGH(PIECTRL_BASE + PIE_O_IER1) &= MG1_1;
/// Enable Interrupts
Interrupt_clearACKGroup(0xFFFFU);
__asm(" NOP");
EINT;
/// To be sure all contactor's are open when offsets are read in order to obtain the correct value of the offset
if((flag_read_offset_adca == 0) &&
(flag_read_offset_adcc == 0) &&
(engineer_return_contactor_k_line_fc == RETURN_CONTACTOR_OPEN) &&
(engineer_return_contactor_k_pl_fc == RETURN_CONTACTOR_OPEN) &&
(engineer_return_contactor_k_line_batt == RETURN_CONTACTOR_OPEN) &&
(engineer_return_contactor_k_pl_batt == RETURN_CONTACTOR_OPEN))
{
read_offset_at_init_adca();
flag_read_offset_adca = 1;
read_offset_at_init_adcc();
flag_read_offset_adcc = 1;
}
MU_TRAC_BATT_FLT_ACC_SAMPLE = ADC_readResult(ADCARESULT_BASE, ADC_SOC_NUMBER0) + ADC_readResult(ADCARESULT_BASE, ADC_SOC_NUMBER1) + ADC_readResult(ADCARESULT_BASE, ADC_SOC_NUMBER2) + ADC_readResult(ADCARESULT_BASE, ADC_SOC_NUMBER3);
/// Divide by 4 to obtain average value.
MU_TRAC_BATT_FLT_AVG_SAMPLE = (MU_TRAC_BATT_FLT_ACC_SAMPLE >> 2);
MU_FUEL_CELL_FLT_ACC_SAMPLE = ADC_readResult(ADCCRESULT_BASE, ADC_SOC_NUMBER0) + ADC_readResult(ADCCRESULT_BASE, ADC_SOC_NUMBER1) + ADC_readResult(ADCCRESULT_BASE, ADC_SOC_NUMBER2) + ADC_readResult(ADCCRESULT_BASE, ADC_SOC_NUMBER3);
/// Divide by 4 to obtain average value.
MU_FUEL_CELL_FLT_AVG_SAMPLE = (MU_FUEL_CELL_FLT_ACC_SAMPLE >> 2);
MI_L_U_FLT_ACC_SAMPLE = ADC_readResult(ADCCRESULT_BASE, ADC_SOC_NUMBER4) + ADC_readResult(ADCCRESULT_BASE, ADC_SOC_NUMBER5) + ADC_readResult(ADCCRESULT_BASE, ADC_SOC_NUMBER6) + ADC_readResult(ADCCRESULT_BASE, ADC_SOC_NUMBER7);
/// Divide by 4 to obtain average value.
MI_L_U_FLT_AVG_SAMPLE = (MI_L_U_FLT_ACC_SAMPLE >> 2);
MI_L_V_FLT_ACC_SAMPLE = ADC_readResult(ADCARESULT_BASE, ADC_SOC_NUMBER4) + ADC_readResult(ADCARESULT_BASE, ADC_SOC_NUMBER5) + ADC_readResult(ADCARESULT_BASE, ADC_SOC_NUMBER6) + ADC_readResult(ADCARESULT_BASE, ADC_SOC_NUMBER7);
/// Divide by 4 to obtain average value.
MI_L_V_FLT_AVG_SAMPLE = (MI_L_V_FLT_ACC_SAMPLE >> 2);
MI_L_W_FLT_ACC_SAMPLE = ADC_readResult(ADCCRESULT_BASE, ADC_SOC_NUMBER8) + ADC_readResult(ADCCRESULT_BASE, ADC_SOC_NUMBER9) + ADC_readResult(ADCCRESULT_BASE, ADC_SOC_NUMBER10) + ADC_readResult(ADCCRESULT_BASE, ADC_SOC_NUMBER11);
/// Divide by 4 to obtain average value.
MI_L_W_FLT_AVG_SAMPLE = (MI_L_W_FLT_ACC_SAMPLE >> 2);
MI_TRAC_BATT_FLT_ACC_SAMPLE = ADC_readResult(ADCARESULT_BASE, ADC_SOC_NUMBER8) + ADC_readResult(ADCARESULT_BASE, ADC_SOC_NUMBER9) + ADC_readResult(ADCARESULT_BASE, ADC_SOC_NUMBER10) + ADC_readResult(ADCARESULT_BASE, ADC_SOC_NUMBER11);
/// Divide by 4 to obtain average value.
MI_TRAC_BATT_FLT_AVG_SAMPLE = (MI_TRAC_BATT_FLT_ACC_SAMPLE >> 2);
MU_FUEL_CELL_PCH_FLT_ACC_SAMPLE = ADC_readResult(ADCARESULT_BASE, ADC_SOC_NUMBER12) + ADC_readResult(ADCARESULT_BASE, ADC_SOC_NUMBER13);
/// Divide by 2 to obtain average value.
MU_FUEL_CELL_PCH_FLT_AVG_SAMPLE = (MU_FUEL_CELL_PCH_FLT_ACC_SAMPLE >> 1);
MU_TRAC_BATT_FLT_ACC_SAMPLE = ADC_readResult(ADCCRESULT_BASE, ADC_SOC_NUMBER12) + ADC_readResult(ADCCRESULT_BASE, ADC_SOC_NUMBER13);
/// Divide by 2 to obtain average value.
MU_TRAC_BATT_PCH_FLT_AVG_SAMPLE = (MU_TRAC_BATT_FLT_ACC_SAMPLE >> 1);
REF_MI_H_2V5_ACC_SAMPLE = ADC_readResult(ADCARESULT_BASE, ADC_SOC_NUMBER14) + ADC_readResult(ADCARESULT_BASE, ADC_SOC_NUMBER15);
/// Divide by 2 to obtain average value.
REF_MI_H_2V5_AVG_SAMPLE = (REF_MI_H_2V5_ACC_SAMPLE >> 1);
MT_COLD_PLATE_FLT_ACC_SAMPLE = ADC_readResult(ADCCRESULT_BASE, ADC_SOC_NUMBER14) + ADC_readResult(ADCCRESULT_BASE, ADC_SOC_NUMBER15);
/// Divide by 2 to obtain average value.
MT_COLD_PLATE_FLT_AVG_SAMPLE = (MT_COLD_PLATE_FLT_ACC_SAMPLE >> 1);
/// Check if overflow has occurred
if(ADC_getInterruptOverflowStatus(ADCA_BASE, ADC_INT_NUMBER1) == true)
{
ADC_clearInterruptOverflowStatus(ADCA_BASE, ADC_INT_NUMBER1);
ADC_clearInterruptStatus(ADCA_BASE, ADC_INT_NUMBER1);
}
/// Clear the interrupt flag
ADC_clearInterruptStatus(ADCA_BASE, ADC_INT_NUMBER1);
/// Acknowledge the interrupt, see PIE Interrupt Vectors table
Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP1);
/// Disable interrupts and restore registers saved:
DINT;
HWREGH(PIECTRL_BASE + PIE_O_IER1) = tempPIEIER;
GPIO_writePin(4, 0); // for test
}__interrupt void isr_slow_tasks()
{
GPIO_writePin(39, 1); // for test
/// Save IER register on stack
volatile uint16_t tempPIEIER = HWREGH(PIECTRL_BASE + PIE_O_IER1);
/// Set the global and group priority to allow CPU interrupts with higher priority
IER |= M_INT1;
IER &= MINT1;
HWREGH(PIECTRL_BASE + PIE_O_IER1) &= MG1_7;
/// Enable Interrupts
Interrupt_clearACKGroup(0xFFFFU);
__asm(" NOP");
EINT;
if(CPUTimer_getTimerOverflowStatus(CPUTIMER0_BASE) == true)
{
CPUTimer_clearOverflowFlag(CPUTIMER0_BASE);
}
/// Update data and send frames if CAN request is detected.
can_request();
/// Read engineer variables and if request by user's is detected.
engineer_variable_and_request_forcing();
/// CMPSS monitoring to detect if protection is set.
cmpss_and_cold_plate_monitoring();
/// Driver return monitoring to detect if protection is set.
drv_monitoring();
/// See requirement REQ_SYST0038
//detection_coldplate(cold_plate_pin, &cold_plate_detect, &cold_plate_state_error, &cold_plate_state);
/// See requirement REQ_SYST0039
//detection_contactor(&k_line_batt, &k_line_batt_state_error, &trigger_state_kline_batt, &trigger_flag_kline_batt, &untrigger_flag_kline_batt);
/// See requirement REQ_SYST0040
//detection_contactor(&k_line_fuel_cell, &k_line_fc_state_error, &trigger_state_kline_fc, &trigger_flag_klinefc, &untrigger_flag_klinefc);
/// See requirement REQ_SYST0041
//detection_contactor(&k_pl_batt, &k_pl_batt_state_error, &trigger_state_kpl_batt, &trigger_flag_kpl_batt, &untrigger_flag_kpl_batt );
/// See requirement REQ_SYST0042
//detection_contactor(&k_pl_fuel_cell, &k_pl_fc_state_error, &trigger_state_kpl_fc, &trigger_flag_kpl_fc, &untrigger_flag_kpl_fc);
/// Get authorization for open contactor's if converter's are off since delay.
get_open_contactor_authorization(&open_contactor, &ack_inh_converter, &open_contactor_authorization);
/// Get authorization for close contactor's if converter's are off since delay and no monitoring are activate.
get_close_k_pl_contactor_authorization(&close_contactor, &step_global, &close_k_pl_authorization);
/// Actions at the state machine due to detection at the contactor's.
contactor_monitoring();
/// State machine
sm_main();
/// Detect if a request to exit RUN state is detected (stop or no loop choice or vehicle crash is nok or consign < min).
request_to_exit_run_state();
/// Acknowledge the interrupt, see PIE Interrupt Vectors table
Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP1);
/// Disable interrupts and restore registers saved:
DINT;
HWREGH(PIECTRL_BASE + PIE_O_IER1) = tempPIEIER;
GPIO_writePin(39, 0); // for test
}#ifndef PRIORITIZED_ISR_LEVELS_H
#define PRIORITIZED_ISR_LEVELS_H
#ifdef __cplusplus
extern "C" {
#endif
//
// Include the header file with software interrupt prioritization logic
//
#include "sw_interrupt_prioritization_logic.h"
//
// Mask for interrupt groups
//
#define M_INT1 0x0001 // INT1 Mask
#define M_INT2 0x0002 // INT2 Mask
#define M_INT3 0x0004 // INT3 Mask
#define M_INT4 0x0008 // INT4 Mask
#define M_INT5 0x0010 // INT5 Mask
#define M_INT6 0x0020 // INT6 Mask
#define M_INT7 0x0040 // INT7 Mask
#define M_INT8 0x0080 // INT8 Mask
#define M_INT9 0x0100 // INT9 Mask
#define M_INT10 0x0200 // INT10 Mask
#define M_INT11 0x0400 // INT11 Mask
#define M_INT12 0x0800 // INT12 Mask
#define M_INT13 0x1000 // INT13 Mask
#define M_INT14 0x2000 // INT14 Mask
#define M_DLOG 0x4000 // DLOGINT Mask
#define M_RTOS 0x8000 // RTOSINT Mask
//
// Interrupt Enable Register Allocation:
// Interrupts can be enabled/disabled using the CPU interrupt enable register
// (IER) and the PIE interrupt enable registers (PIEIER1 to PIEIER12).
//
//
// Set "Global" Interrupt Priority Level (IER register):
//
// The user must set the appropriate priority level for each of the CPU
// interrupts. This is termed as the "global" priority. The priority level
// must be a number between 1 (highest) to 16 (lowest). A value of 0 must
// be entered for reserved interrupts or interrupts that are not used.
//
// Note: The priority levels below are used to calculate the IER register
// interrupt masks MINT1 to MINT16.
//
// Note: The priority levels shown here may not make sense in a
// real application. This is for demonstration purposes only!!!
//
// The user should change these to values that make sense for
// their application.
//
// 0 = not used
// 1 = highest priority
// ...
// 16 = lowest priority
//
#define INT1PL 3 // Global Priority for Group1 Interrupts
#define INT2PL 1 // Global Priority for Group2 Interrupts
#define INT3PL 2 // Global Priority for Group3 Interrupts
#define INT4PL 0 // Global Priority for Group4 Interrupts
#define INT5PL 0 // Global Priority for Group5 Interrupts
#define INT6PL 0 // Global Priority for Group6 Interrupts
#define INT7PL 0 // Global Priority for Group7 Interrupts
#define INT8PL 0 // Global Priority for Group8 Interrupts
#define INT9PL 0 // Global Priority for Group9 Interrupts
#define INT10PL 0 // Global Priority for Group10 Interrupts
#define INT11PL 0 // Global Priority for Group11 Interrupts
#define INT12PL 0 // Global Priority for Group12 Interrupts
#define INT13PL 0 // Global Priority for INT13 (TINT1)
#define INT14PL 0 // Global Priority for INT14 (TINT2)
#define INT15PL 0 // Global Priority for DATALOG
#define INT16PL 0 // Global Priority for RTOSINT
//
// Set "Group" Interrupt Priority Level (PIEIER1 to PIEIER12 registers):
//
// The user must set the appropriate priority level for each of the PIE
// interrupts. This is termed as the "group" priority. The priority level
// must be a number between 1 (highest) to 16 (lowest). A value of 0 must
// be entered for reserved interrupts or interrupts that are not used.
//
// Note: The priority levels below are used to calculate the following
// PIEIER register interrupt masks:
// MG1_1 to MG1_16
// MG2_1 to MG2_16
// MG3_1 to MG3_16
// MG4_1 to MG4_16
// MG5_1 to MG5_16
// MG6_1 to MG6_16
// MG7_1 to MG7_16
// MG8_1 to MG8_16
// MG9_1 to MG9_16
// MG10_1 to MG10_16
// MG11_1 to MG11_16
// MG12_1 to MG12_16
//
// Note: The priority levels shown here may not make sense in a
// real application. This is for demonstration purposes only!!!
//
// The user should change these to values that make sense for
// their application.
//
// 0 = not used
// 1 = highest priority
// ...
// 16 = lowest priority
//
#define G1_1PL 1 // ADCA1_INT
#define G1_2PL 0 // Reserved
#define G1_3PL 0 // ADCC1_INT
#define G1_4PL 0 // XINT1_INT
#define G1_5PL 0 // XINT2_INT
#define G1_6PL 0 // Reserved
#define G1_7PL 2 // TIMER0_INT
#define G1_8PL 0 // WAKE_INT
#define G1_9PL 0 // Reserved
#define G1_10PL 0 // Reserved
#define G1_11PL 0 // Reserved
#define G1_12PL 0 // Reserved
#define G1_13PL 0 // Reserved
#define G1_14PL 0 // Reserved
#define G1_15PL 0 // Reserved
#define G1_16PL 0 // Reserved
#define G2_1PL 1 // EPWM1_TZ_INT
#define G2_2PL 2 // EPWM2_TZ_INT
#define G2_3PL 0 // EPWM3_TZ_INT
#define G2_4PL 3 // EPWM4_TZ_INT
#define G2_5PL 0 // EPWM5_TZ_INT
#define G2_6PL 0 // EPWM6_TZ_INT
#define G2_7PL 0 // EPWM7_TZ_INT
#define G2_8PL 0 // Reserved
#define G2_9PL 0 // Reserved
#define G2_10PL 0 // Reserved
#define G2_11PL 0 // Reserved
#define G2_12PL 0 // Reserved
#define G2_13PL 0 // Reserved
#define G2_14PL 0 // Reserved
#define G2_15PL 0 // Reserved
#define G2_16PL 0 // Reserved
#define G3_1PL 0 // EPWM1_INT
#define G3_2PL 0 // EPWM2_INT
#define G3_3PL 1 // EPWM3_INT
#define G3_4PL 0 // EPWM4_INT
#define G3_5PL 0 // EPWM5_INT
#define G3_6PL 0 // EPWM6_INT
#define G3_7PL 0 // EPWM7_INT
#define G3_8PL 0 // Reserved
#define G3_9PL 0 // Reserved
#define G3_10PL 0 // Reserved
#define G3_11PL 0 // Reserved
#define G3_12PL 0 // Reserved
#define G3_13PL 0 // Reserved
#define G3_14PL 0 // Reserved
#define G3_15PL 0 // Reserved
#define G3_16PL 0 // Reserved
#define G4_1PL 0 // ECAP1_INT
#define G4_2PL 0 // ECAP2_INT
#define G4_3PL 0 // ECAP3_INT
#define G4_4PL 0 // Reserved
#define G4_5PL 0 // Reserved
#define G4_6PL 0 // Reserved
#define G4_7PL 0 // Reserved
#define G4_8PL 0 // Reserved
#define G4_9PL 0 // Reserved
#define G4_10PL 0 // Reserved
#define G4_11PL 0 // ECAP3_2_INT
#define G4_12PL 0 // Reserved
#define G4_13PL 0 // Reserved
#define G4_14PL 0 // Reserved
#define G4_15PL 0 // Reserved
#define G4_16PL 0 // Reserved
#define G5_1PL 0 // EQEP1_INT
#define G5_2PL 0 // EQEP2_INT
#define G5_3PL 0 // Reserved
#define G5_4PL 0 // Reserved
#define G5_5PL 0 // CLB1_INT
#define G5_6PL 0 // CLB2_INT
#define G5_7PL 0 // Reserved
#define G5_8PL 0 // Reserved
#define G5_9PL 0 // Reserved
#define G5_10PL 0 // Reserved
#define G5_11PL 0 // Reserved
#define G5_12PL 0 // Reserved
#define G5_13PL 0 // Reserved
#define G5_14PL 0 // Reserved
#define G5_15PL 0 // Reserved
#define G5_16PL 0 // Reserved
#define G6_1PL 0 // SPIA_RX_INT
#define G6_2PL 0 // SPIA_TX_INT
#define G6_3PL 0 // SPIB_RX_INT
#define G6_4PL 0 // SPIB_TX_INT
#define G6_5PL 0 // Reserved
#define G6_6PL 0 // Reserved
#define G6_7PL 0 // Reserved
#define G6_8PL 0 // Reserved
#define G6_9PL 0 // Reserved
#define G6_10PL 0 // Reserved
#define G6_11PL 0 // Reserved
#define G6_12PL 0 // Reserved
#define G6_13PL 0 // Reserved
#define G6_14PL 0 // Reserved
#define G6_15PL 0 // Reserved
#define G6_16PL 0 // Reserved
#define G7_1PL 0 // DMA_CH1_INT
#define G7_2PL 0 // DMA_CH2_INT
#define G7_3PL 0 // DMA_CH3_INT
#define G7_4PL 0 // DMA_CH4_INT
#define G7_5PL 0 // DMA_CH5_INT
#define G7_6PL 0 // DMA_CH6_INT
#define G7_7PL 0 // Reserved
#define G7_8PL 0 // Reserved
#define G7_9PL 0 // Reserved
#define G7_10PL 0 // Reserved
#define G7_11PL 0 // FSITXA1_INT
#define G7_12PL 0 // FSITXA2_INT
#define G7_13PL 0 // FSIRXA1_INT
#define G7_14PL 0 // FSIRXA2_INT
#define G7_15PL 0 // Reserved
#define G7_16PL 0 // DCC0_INT
#define G8_1PL 0 // I2CA_INT
#define G8_2PL 0 // I2CA_FIFO_INT
#define G8_3PL 0 // I2CB_INT
#define G8_4PL 0 // I2CB_FIFO_INT
#define G8_5PL 0 // Reserved
#define G8_6PL 0 // Reserved
#define G8_7PL 0 // Reserved
#define G8_8PL 0 // Reserved
#define G8_9PL 0 // LINA0_INT
#define G8_10PL 0 // LINA1_INT
#define G8_11PL 0 // LINB0_INT
#define G8_12PL 0 // LINB1_INT
#define G8_13PL 0 // PMBUSA_INT
#define G8_14PL 0 // Reserved
#define G8_15PL 0 // Reserved
#define G8_16PL 0 // DCC1_INT
#define G9_1PL 0 // SCIA_RX_INT
#define G9_2PL 0 // SCIA_TX_INT
#define G9_3PL 0 // Reserved
#define G9_4PL 0 // Reserved
#define G9_5PL 0 // CANA0_INT
#define G9_6PL 0 // CANA1_INT
#define G9_7PL 0 // Reserved
#define G9_8PL 0 // Reserved
#define G9_9PL 0 // Reserved
#define G9_10PL 0 // Reserved
#define G9_11PL 0 // Reserved
#define G9_12PL 0 // Reserved
#define G9_13PL 0 // BGCRC_INT
#define G9_14PL 0 // Reserved
#define G9_15PL 0 // Reserved
#define G9_16PL 0 // HICA_INT
#define G10_1PL 0 // ADCA_EVT_INT
#define G10_2PL 0 // ADCA2_INT
#define G10_3PL 0 // ADCA3_INT
#define G10_4PL 0 // ADCA4_INT
#define G10_5PL 0 // Reserved
#define G10_6PL 0 // Reserved
#define G10_7PL 0 // Reserved
#define G10_8PL 0 // Reserved
#define G10_9PL 0 // ADCC_EVT_INT
#define G10_10PL 0 // ADCC2_INT
#define G10_11PL 0 // ADCC3_INT
#define G10_12PL 0 // ADCC4_INT
#define G10_13PL 0 // Reserved
#define G10_14PL 0 // Reserved
#define G10_15PL 0 // Reserved
#define G10_16PL 0 // Reserved
#define G11_1PL 0 // Reserved
#define G11_2PL 0 // Reserved
#define G11_3PL 0 // Reserved
#define G11_4PL 0 // Reserved
#define G11_5PL 0 // Reserved
#define G11_6PL 0 // Reserved
#define G11_7PL 0 // Reserved
#define G11_8PL 0 // Reserved
#define G11_9PL 0 // Reserved
#define G11_10PL 0 // Reserved
#define G11_11PL 0 // Reserved
#define G11_12PL 0 // Reserved
#define G11_13PL 0 // Reserved
#define G11_14PL 0 // Reserved
#define G11_15PL 0 // Reserved
#define G11_16PL 0 // Reserved
#define G12_1PL 0 // XINT3_INT
#define G12_2PL 0 // XINT4_INT
#define G12_3PL 0 // XINT5_INT
#define G12_4PL 0 // PBIST_INT
#define G12_5PL 0 // FMC_INT
#define G12_6PL 0 // Reserved
#define G12_7PL 0 // FPU_OVERFLOW_ISR
#define G12_8PL 0 // FPU_UNDERFLOW_ISR
#define G12_9PL 0 // Reserved
#define G12_10PL 0 // RAM_CORRECTABLE_ERROR_ISR
#define G12_11PL 0 // FLASH_CORRECTABLE_ERROR_ISR
#define G12_12PL 0 // RAM_ACCESS_VIOLATION_INT
#define G12_13PL 0 // SYS_PLL_SLIP_INT
#define G12_14PL 0 // Reserved
#define G12_15PL 0 // Reserved
#define G12_16PL 0 // Reserved
#ifdef __cplusplus
}
#endif /* extern "C" */
#endif
Probably a bad setting ? Can you help me please ?
Thanks
Damien