This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28379D: Configuring one MODULE on the board

Part Number: TMS320F28379D
Other Parts Discussed in Thread: C2000WARE

Hi Experts,

Our customer is using TI DSP board F28379D. He is not able to configure one MODULE on the board. He need help regarding the board.

His aim is to operate two parallel inverters with 30 kHz switching frequency.  He is writing in one isr whose clock is 200kHz (5 micro sec). His code execution time is 7 micro sec. To overcome this problem he is trying to configure a dual CPU for faster operation. He is trying to send multiple messages between the two CPUs. For that, he started reading IPC and CLA from the texas instrument reference manual but not able to start. Please guide us.

I hope you can help us. Thank you.

Kind regards,

Gerald