Part Number: TMS320F28388D
Other Parts Discussed in Thread: C2000WARE
Hi experts,
I want to use SDFM with the following settings.(Repeat 1 to 4)
- Start SDFM with period of PWM timer in up-down mode
- Stop SDFM after getting the value in SDFM
- Clear SDFM's buffer
- return to "1"
Is there an SFDM sample program for this specification in C2000ware?
I checked the following folders but could not find it.
C:\ti\c2000\C2000Ware_4_01_00_00\driverlib\f2838x\examples\c28x\sdfm
Since this spec is a common usage in servo control, I assumed these projects were out there somewhere.
Best regards,
Sasaki