Hi,
Please advise which Pins on the 64 pin device can be mapped to the TZ1 TZ2 and TZ2 registers. It is not clear in the technical information I am reading.
Thank you,
William
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Please advise which Pins on the 64 pin device can be mapped to the TZ1 TZ2 and TZ2 registers. It is not clear in the technical information I am reading.
Thank you,
William
Hi William,
Refer to this figure in the crossbar chapter:
TZ1-3 and TZ6 are directly routed to the input XBAR.
Thank you,
Luke
Hi Luke,
I saw that but my confusion is determining which GPIO pins these input XBARS map out to? What pins on the 64-pin TMS320F280039C device are mapped to the Trip Zone signals? Where do I find that information? For example, if I want to configure a GPIO pin to trip a TZ1 fault of the ePWM module, what pin would I wire that fault signal to on the 64-pin device of the TMS320F280039C?
Thank you,
William
Hi William,
Each Input XBAR can connect to any of the GPIOs. This is determined by the INPUTxSELECT registers in the Cross-bar chapter. In the case of TZ1 you would configure INPUT1SELECT.
--Luke