Part Number: TMS320F280049C
Other Parts Discussed in Thread: SYSCONFIG
Peter and friends,
I've got my CLB design working well on a Launchpad and I'm currently integrating my prototype implementation with the rest of my product's firmware. This is requiring me to refactor some peripheral assignments and GPIO muxing and I'm running into some trouble with a creative peripheral pin reassignment.
Here's what I'm trying to accomplish:
EPWM4A -> CLB3 Input 1 -> Out LUT 4 -> Output Xbar 3 -> GPIO 5



I've been able to validate part of this signal chain by observing the state of GPIO 5 and changing the value of the CLB_OUTPUT_LUT_4 register such that it had a static output (0x00550000 or 0x00550008). I was able to successfully wiggle the pin this way, which would indicate the connectivity between the out LUT and the GPIO through the output xbar is good.
I'm now trying to validate the signal coming into the CLB. I have some other PWM signals which I can observe externally so I've tried using those as the source instead of EPWM4A. For instance, EPWM2B comes out externally so I view that with a scope as well as GPIO5 and I configure input 1 on CLB 3 to be sourced from EPWM2B using the global mux. When I do this, I see the EPWM2B on its normal pin (GPIO3), but I do not see any signal on GPIO5 (it's just low). Repeating the experiment from the previous paragraph, I can still wiggle the pins. Any ideas as to what I might be doing wrong?
Best,
Trey