Other Parts Discussed in Thread: TMS320F28335, TIDM-1022
Hello, I use TMS320F28335 chip to control single-phase Boost PFC. The control algorithm adopts double loop PID control of voltage loop and current loop. At present, the test parameters of single-phase Boost PFC are: input 20VAC during low-voltage test, set output 50VDC, load 100 ohm, switching frequency 100kHz double loop program. Sampling ratio: input voltage hardware ratio is 5.1k/605.1k, inductance current sampling ratio is 499/1200, and output voltage sampling ratio is 2.4k/402.4k. Program: Set two PWM, wherein the PWM1 cycle is 100kHz, trigger ADC sampling (all variables take a point in the switching cycle), ADC triggers the interrupt function, and run the double loop PID control program in the interrupt function. During the test, the PWM duty cycle is 0 or the maximum value set for the current loop. As shown in the figure, purple is the input current, light blue is the drive signal waveform, and dark blue is the input voltage waveform. What may be the problem?

void main()
{
InitSysCtrl();
MemCopy(&RamfuncsLoadStart, &RamfuncsLoadEnd, &RamfuncsRunStart);
InitFlash();
EALLOW;
SysCtrlRegs.HISPCP.all = ADC_MODCLK;
EDIS;
DINT;
InitEPwm1Gpio();
InitEPwm2Gpio();
InitPieCtrl();
IER = 0x0000;
IFR = 0x0000;
InitPieVectTable();
EALLOW;
PieVectTable.ADCINT = &adc_isr;
EDIS;
InitAdc();
PieCtrlRegs.PIEIER1.bit.INTx6 = 1;
IER |= M_INT1; // Enable CPU Interrupt 1
EINT;// Enable Global interrupt INTM
ERTM;// Enable Global realtime interrupt DBGM
EALLOW;
SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 0;
SysCtrlRegs.PCLKCR1.bit.EPWM1ENCLK = 1;
SysCtrlRegs.PCLKCR1.bit.EPWM2ENCLK = 1;
EDIS;
InitADC();
InitEPwm1Example();
InitEPwm2Example();
Disable_boost_PWM();
EALLOW;
SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 1;
EDIS;
for (;;)
{
}
}
void InitEPwm1Example()
{
EPwm1Regs.TBPRD = 750;
EPwm1Regs.TBPHS.half.TBPHS = 0x00;
EPwm1Regs.TBCTR = 0x0000;
EPwm1Regs.TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN;
EPwm1Regs.TBCTL.bit.PHSEN = TB_DISABLE;
EPwm1Regs.TBCTL.bit.SYNCOSEL = TB_CTR_ZERO;
EPwm1Regs.TBCTL.bit.HSPCLKDIV =0x00;
EPwm1Regs.TBCTL.bit.CLKDIV = 0x00;
EPwm1Regs.DBCTL.bit.IN_MODE =0;
EPwm1Regs.DBCTL.bit.POLSEL =2;
EPwm1Regs.DBCTL.bit.OUT_MODE =3;
EPwm1Regs.CMPCTL.bit.SHDWAMODE = CC_CTR_ZERO;
EPwm1Regs.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO;
EPwm1Regs.CMPA.half.CMPA = 750;
EPwm1Regs.AQCTLA.bit.ZRO = AQ_SET;
EPwm1Regs.AQCTLA.bit.CAU = AQ_CLEAR;
EALLOW;
// What do we want the TZ1 and TZ2 to do?
EPwm1Regs.TZCTL.bit.TZA = TZ_FORCE_LO;
EPwm1Regs.TZCTL.bit.TZB = TZ_FORCE_LO;
// Enable TZ interrupt
EPwm1Regs.TZEINT.bit.OST = 1;
EDIS;
//(Q:用于触发ADC转换)
EPwm1Regs.ETSEL.bit.SOCAEN = 1;
EPwm1Regs.ETSEL.bit.SOCASEL = 2;
EPwm1Regs.ETPS.bit.SOCAPRD = 1;
}
void InitEPwm2Example()
{
EPwm2Regs.TBPRD = 750;
EPwm2Regs.TBPHS.half.TBPHS = 0x00;
EPwm2Regs.TBCTR = 0x0000;
EPwm2Regs.TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN ;
EPwm2Regs.TBCTL.bit.PHSEN = TB_DISABLE;
EPwm2Regs.TBCTL.bit.SYNCOSEL = TB_CTR_ZERO;
EPwm2Regs.TBCTL.bit.HSPCLKDIV =0x00;
EPwm2Regs.TBCTL.bit.CLKDIV = 0x00;
EPwm2Regs.DBCTL.bit.IN_MODE =0;
EPwm2Regs.DBCTL.bit.POLSEL =2;
EPwm2Regs.DBCTL.bit.OUT_MODE =3;
EPwm2Regs.CMPCTL.bit.SHDWAMODE = CC_CTR_ZERO;
EPwm2Regs.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO;
EPwm2Regs.CMPA.half.CMPA = GD_EPWM1_CAMPA1;
EPwm2Regs.AQCTLA.bit.CAD = AQ_SET;
EPwm2Regs.AQCTLA.bit.CAU = AQ_CLEAR;
EALLOW;
// What do we want the TZ1 and TZ2 to do?
EPwm2Regs.TZCTL.bit.TZA = TZ_FORCE_LO;
EPwm2Regs.TZCTL.bit.TZB = TZ_FORCE_LO;
// Enable TZ interrupt
EPwm2Regs.TZEINT.bit.OST = 1;
EDIS;
}
void InitADC()
{
AdcRegs.ADCTRL1.bit.CPS = 1;
AdcRegs.ADCTRL3.bit.ADCCLKPS = ADC_CKPS;
AdcRegs.ADCTRL1.bit.ACQ_PS = ADC_SHCLK;
AdcRegs.ADCTRL1.bit.SEQ_CASC = 1;
AdcRegs.ADCTRL1.bit.SEQ_OVRD = 0;
AdcRegs.ADCTRL1.bit.CONT_RUN = 0;
AdcRegs.ADCTRL3.bit.SMODE_SEL = 0;
AdcRegs.ADCMAXCONV.bit.MAX_CONV1 = 0x4;
AdcRegs.ADCCHSELSEQ1.bit.CONV00=0x02;
AdcRegs.ADCCHSELSEQ1.bit.CONV01=0x03;
AdcRegs.ADCCHSELSEQ1.bit.CONV02=0x04;
AdcRegs.ADCCHSELSEQ1.bit.CONV03=0x05;
AdcRegs.ADCTRL2.bit.EPWM_SOCA_SEQ1 = 1;
AdcRegs.ADCTRL2.bit.INT_ENA_SEQ1 = 1;
AdcRegs.ADCTRL2.bit.INT_MOD_SEQ1 = 0;
}
interrupt void adc_isr()
{
while(AdcRegs.ADCST.bit.INT_SEQ1==0) {}
Value_Detection();
Enable_boost_PWM();
rectify_vac();
handle_voltage_loop();
calculate_current_target_shunt();
current_PIcontrol();
GD_EPWM1_CAMPA1=(int) (750.0 * Current_Output1);
EPwm2Regs.CMPA.half.CMPA = GD_EPWM1_CAMPA1;
EPwm1Regs.ETCLR.bit.SOCA = 1;
AdcRegs.ADCTRL2.bit.RST_SEQ1 = 1; // Reset SEQ1
PieCtrlRegs.PIEACK.all = PIEACK_GROUP1; // Acknowledge interrupt to PIE
AdcRegs.ADCST.bit.INT_SEQ1_CLR=1;
return;
}
void Value_Detection()
{
SampleTable0 = ( (AdcRegs.ADCRESULT0)>>4); //Vl
SampleTable1 = ( (AdcRegs.ADCRESULT1)>>4); //VN
SampleTable2 = ( (AdcRegs.ADCRESULT2)>>4); //IL
SampleTable3 = ( (AdcRegs.ADCRESULT3)>>4); //VO
value_temp1 = SampleTable0 *(2017.0/23205.0) ;
Sample_vl = value_temp1 ;
value_temp2 = SampleTable1 *(2017.0/23205.0) ;
Sample_vn = value_temp2 ;
value_temp3 = SampleTable2 *(80.0/45409.0);
Sample_il = value_temp3 ;
value_temp4 = SampleTable3 *(503.0/4095.0);
Sample_vo = value_temp4 ;
}
void rectify_vac ()
{
if (Sample_vl > Sample_vn )
{
Vin_raw = Sample_vl - Sample_vn;
Vin_positive = 1.0;
}
else //cycle for neutral
{
Vin_raw = Sample_vn - Sample_vl;
Vin_positive = 0.0;
}
Vin_sum = Vin_raw + Vin_sum - (Vin_sum * 0.25);
Vin_filtered = Vin_sum * 0.25;
Vin_squared = (Vin_filtered * Vin_filtered);
}
void handle_voltage_loop()
{
Current_i_target_average = proportional_integral(50.0 - Sample_vo);
}
float proportional_integral(float voltage_Error)
{
Voltage_Error = voltage_Error;
Voltage_Output1=0.01 *(Voltage_Error-Voltage_Error11) + 1.0 * Voltage_Error ;
Voltage_Output = Voltage_Output + Voltage_Output1 ;
if ( Voltage_Output > 1.4 )
{
Voltage_Output = 1.4;
}
else if ( Voltage_Output <= 0.0 )
{
Voltage_Output =0.0;
}
Voltage_Error11 = Voltage_Error ;
return Voltage_Output;
}
void calculate_current_target_shunt()
{
Current_i_target_sensed = (( Current_i_target_average * Vin_filtered )/20.0);
if(Current_i_target_sensed > 2.0)
{
Current_i_target_sensed = 2.0 ;
}
else if(Current_i_target_sensed < 0.0)
{
Current_i_target_sensed = 0.0 ;
}
}
void current_PIcontrol()
{
Current_Error1 = Current_i_target_sensed - Sample_il ;
Current_Output11 = 1.5 *( Current_Error1-Current_Error11) + 600.0 * Current_Error1;//KP=1.5,KI=600
Current_Output1 = Current_Output1 + Current_Output11 ;
if ( Current_Output1 > 0.9 )
{
Current_Output1=0.9 ;
}
else if( Current_Output1 <=0.0 )
{
Current_Output1=0.0 ;
}
Current_Error11 = Current_Error1 ;
}
void Disable_boost_PWM()
{
EALLOW;
GpioCtrlRegs.GPAMUX1.bit.GPIO2 = 0;
GpioCtrlRegs.GPADIR.bit.GPIO2 = 1;
GpioCtrlRegs.GPAMUX1.bit.GPIO3 = 0;
GpioCtrlRegs.GPADIR.bit.GPIO3 = 1;
EDIS;
GpioDataRegs.GPACLEAR.bit.GPIO2=1;
GpioDataRegs.GPACLEAR.bit.GPIO3=1;
}
void Enable_boost_PWM()
{
EALLOW;
GpioCtrlRegs.GPAMUX1.bit.GPIO2 = 1;
GpioCtrlRegs.GPADIR.bit.GPIO2 = 1;
GpioCtrlRegs.GPAMUX1.bit.GPIO3 = 1;
GpioCtrlRegs.GPADIR.bit.GPIO3 = 1;
EDIS;
}