Other Parts Discussed in Thread: ADS8363
I would like to interface ADS8363 evaluation model to Piccolo control stick through the SPI interface.
Can the SPI interface handle 16 Mbits/ second?
What is the max speed SPI can handle in Piccolo?
Can the Piccolo USB interface handle 16 Mbits/ second?
What is the maximum speed USb can handle?
For some reason I could not post this in IE9 and had to post it in Safari!