Other Parts Discussed in Thread: CONTROLSUITE
Hello,
I have background of motor control with tms320f2812eZdsp.
1. I want to use serial peripheral interface to connect to DAC AD5662. this is a single way communication.
Can some one help me please with a sample serial peripheral interface code for the f28069 Control Stick?
I think i need to use SPISIMOA (24) , SPICLKA ( 29 ) and a pin to sync the communication.
-----------------------------------------------------------------------------------------------------------------------------------------------------------------------------------
2. I want to develop a GUI in windows, to communicate the position ref to the control stick and read the position from the control stick. A sample development idea or code will be really helpful.
Thanks and Best Regards,
Shantanu.