Part Number: TMS320LF2407A
Hi TI
Problem description:
- 100 PCBs were welded, 10 PCBs reported errors when downloading the program for the first time, and 90 PCBs could be downloaded normally;
- Download the boards that report errors:
7 boards report password errors (Figure 1), 3 boards appear to have programs (Figure 2), and 0X0001 errors are reported when executing Clear, as shown in Figure 3 and Figure 4.
Need help to confirm:
From the above 10 abnormal boards downloaded, can it be determined that the internal program of the chip is caused?
Figure 1:

Figure 2:

Figure 3:

Figure 4: