Part Number: INSTASPIN-BLDC
Other Parts Discussed in Thread: TMS320F28379D, TMDXIDDK379D, C2000WARE
Hi,
We are designing a 10kW bidirectional inverter that is to drive a 30 V, 250 A, motor running at 135000rpm. Typically the input is 48V DC and it is a turbo drive inverter for diesel engine.
I want to know what is the max frequency that InstaSpin can support with and without encoder and the max capacity of the eQEP module that Ti has.
Kindly revert asap.
Thanks and regards
Mohana Lakshmi J