Hi team,
Here's an issue from the customer may need your help:



Why is IER cleared after the CPU saves its context on the stack? If cleared, the interrupt signal is disconnected from the CPU.
"Writes to IER and INTM are atomic operations", does this refer to the CPU automatically operate two bits? Manual does not seem to mention when IER will be set again.
When using this bit, the IER bit is normally set in initialization, right? If the IER bit is cleared after the save context, the user needs to add instructions to set it again. The customer did not change the IER status again when coding.
Could you help check this case? Thanks.
Best Regards,
Cherry