Part Number: C2000WARE-MOTORCONTROL-SDK
Other Parts Discussed in Thread: C2000WARE
Hi Experts,
Seeking your assistance as we have some points that need to clarify.
[1] As I understand it's a kind of firmware embedded inside some devices correctly? I am speaking here about FAST.
[2] I need to know what devices exactly include FAST.
[3] Are there Dependencies between InstaSpin and CLA existence?
[4] I need to confirm that to adapt my project with instaspin solution I will need to measure the phase volts also as input to the SW from ADC , or there is some workaround that allows me to pass the Volt by some SW function if I was able to get the volt from the current already measured?
[5] Also, would you please also confirm with me is there any way to use "C2000WARE-MOTORCONTROL-SDK" to control sensorless motors using FOC without usage of instaSPIN Approach?
Hope to hear an update from experts for us in order to decide microcontroller to be used and the impact on our HW design.
Regards,
Archie A.