Part Number: TMS320F280040-Q1
Hello,
I am trying to load the program and let it run from the flash. And got this issue.
After the program is loaded to the flash and then the program starts running on flash. Everything works find. But once the power is recycled, the serial communication stops working properly any more. The MCU Tx line has no signal and PC terminal is not displaying anything, but the program is running and MCU Rx is still receiving message from the PC keyboard. Both Tx and Rx’s idle signals are fine. Do a soft reset the serial communication stays the same.
Anyone has experience with this scenario and knows if there is potentially anything wrong with loading the program or the serial communication?
Thanks!
Crane