This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280025C: spruin7a Missing UID_REGS Base address

Part Number: TMS320F280025C


As stated in the title Table 3-19 does not list UID regs.  No where in the driverlib or bitfield header collateral is the base address mentioned.  Additionally, these registers are not shown in the CCS register window as far as I can tell.

The datasheet does have the address of the UID_UNIQUE register, but unless UID_REGS is at an address that doesn't end with 0, it seems to me like either the offset or the address may be incorrect.

Soooo C2k experts, what is the base address of UID_REGs on F28002x?? Is it 0x701E8?

Trey