Part Number: TMS320F28027
Other Parts Discussed in Thread: C2000WARE
Hi,
I am trying to create a new project for a TMS320F28027. I created a new CCS project and included the header file for DSP28x_Project.h which includes all the peripheral header files. I tried adding a gpio_init() function to the main file to initialize GPIOs. However it is giving me an error that it cannot resolve _GpioCtrlRegs. I am not sure what is incorrect as I am able to use the GpioCtrlRegs and the code is automatically able to lookup elements of the structure. Any suggestions would be really helpful.
Thank you,
Aditya
Error in the console:
undefined first referenced
symbol in file
--------- ----------------
_GpioCtrlRegs ./f2802x_gpio.obj
error #10234-D: unresolved symbols remain
error #10010: errors encountered during linking; "2802xTestProject.out" not built
>> Compilation failure
makefile:144: recipe for target '2802xTestProject.out' failed
gmake[1]: *** [2802xTestProject.out] Error 1
makefile:140: recipe for target 'all' failed
gmake: *** [all] Error 2