Part Number: TMDSCNCD28379D
I have a controlCARD with firmware on it that I need to save in a way that I can put that firmware onto another controlCARD without erasing/changing the firmware on the original controlCARD. I've seen another user's post about this same topic, but it was from over 10 years ago, and the links in the answer no longer work. Is the Memory Save/Load Utility still available? How would it be used in this circumstance?
Thank you!
Here's my system specs:
Code Composer Studio
Version: 12.0.0.00009
OS: Windows 10, v.10.0, x86_64 / win32
Java vendor: Eclipse Adoptium
Java runtime version: 11.0.13+8
Java version: 11.0.13