Part Number: TMS320F280025C
Hi,
I've a issue with the event trigger interrupt generation, I want generate an interrupt triggered by ePWM1 when CTR = 0. So you can see my configuration bellow.
And question : ETSEL.INTSEL equal 1 so it's good for CTR = 0 and INTEN = 1 to enable interrupt. Problem with the ETPS config I want to select ETPS.INTPRD because I want to generate event at each trigger.
So ETPS.INTPRD will be equal to 1 no ? and in the CCS window debugger you can see ETPS.INTPRD = 0. How select this bit by driverlib please ? because this function EPWM_setInterruptEventCount(EPWM1_BASE, 1) select ETINTPS.INTPRD2.
What's the problem with my configuration because I see shift timing between ePWM1 and INT_EPWM1 ? I want synchronize ePWM1 rising edge with INTePWM1 rising edge.
Pink signal : ePWM1
Yellow signal : INT_EPWM1 (1 enter in interrupt, 0 out)
What's the different between ETPS.INTPRD and ETINTPS.INTPRD2 if I select interrupt at each event ?
#include "device.h"
__interrupt void isr_read_adc(void);
void main(void)
{
/// Initialize device clock and peripherals
Device_init();
/// Disable pin locks and enable internal pullups.
Device_initGPIO();
/// Initialize PIE and clear PIE (for pie multiplexer) and IFR (for cpu) registers (IER for pie table).
Interrupt_initModule();
/// Initialize the PIE vector table with pointers to the shell Interrupt Service Routines (ISR).
Interrupt_initVectorTable();
/// Disable sync and clock to PWM
SysCtl_disablePeripheral(SYSCTL_PERIPH_CLK_TBCLKSYNC);
/// Parameters
EPWM_setTimeBaseCounterMode(EPWM1_BASE, EPWM_COUNTER_MODE_UP);
EPWM_setTimeBaseCounter(EPWM1_BASE, 0U);
/// To have around 0.05% (See ePWM chapter in Chapter 17 Technical reference manual page 1798) do point for ePWM precision who is the maximum precision with the ePWM module.
/// If we want more precision use the HRPWM module.
EPWM_setClockPrescaler(EPWM1_BASE, EPWM_CLOCK_DIVIDER_1, EPWM_HSCLOCK_DIVIDER_1);
/// Set up shadowing
EPWM_setCounterCompareShadowLoadMode(EPWM1_BASE, EPWM_COUNTER_COMPARE_A, EPWM_COMP_LOAD_ON_CNTR_ZERO);
/// Set actions for boost assembly
EPWM_setActionQualifierAction(EPWM1_BASE, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_HIGH, EPWM_AQ_OUTPUT_ON_TIMEBASE_UP_CMPA);
EPWM_setActionQualifierAction(EPWM1_BASE, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_LOW, EPWM_AQ_OUTPUT_ON_TIMEBASE_ZERO);
/// For buck assembly
EPWM_setActionQualifierAction(EPWM1_BASE, EPWM_AQ_OUTPUT_B, EPWM_AQ_OUTPUT_HIGH, EPWM_AQ_OUTPUT_ON_TIMEBASE_UP_CMPB);
EPWM_setActionQualifierAction(EPWM1_BASE, EPWM_AQ_OUTPUT_B, EPWM_AQ_OUTPUT_LOW, EPWM_AQ_OUTPUT_ON_TIMEBASE_ZERO);
EPWM_setTimeBasePeriod(EPWM1_BASE, 2499);
EPWM_setCounterCompareValue(EPWM1_BASE, EPWM_COUNTER_COMPARE_B, 1250);
/// Interrupt where we will change the Compare Values
/// Select INT on Time base counter zero event,
/// Enable INT, generate INT on 1rd event
EPWM_setInterruptSource(EPWM1_BASE, EPWM_INT_TBCTR_ZERO);
EPWM_enableInterrupt(EPWM1_BASE);
/// To trigger the interrupt at each event, maximum value equal to 15.
EPWM_setInterruptEventCount(EPWM1_BASE, 1);
EPWM_setPhaseShift(EPWM1_BASE, 0);
EPWM_disablePhaseShiftLoad(EPWM1_BASE);
GPIO_setPinConfig(GPIO_42_GPIO42);
GPIO_setDirectionMode(42, GPIO_DIR_MODE_OUT);
GPIO_setPadConfig(42, GPIO_PIN_TYPE_STD);
GPIO_writePin(42, 0);
/// GPIO initialization EPWM1
EALLOW;
GPIO_setPinConfig(GPIO_0_EPWM1_A);
GPIO_setPinConfig(GPIO_1_EPWM1_B);
EDIS;
Interrupt_register(INT_EPWM1, &isr_read_adc);
Interrupt_enable(INT_EPWM1);
/// Enable sync and clock to PWM
SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_TBCLKSYNC);
/// Enable Global Interrupt (INTM) and realtime interrupt (DBGM)
EINT;
ERTM;
while(1)
{
}
}
__interrupt void isr_read_adc(void)
{
EPWM_clearEventTriggerInterruptFlag(EPWM1_BASE);
GPIO_writePin(42, 1);
DEVICE_DELAY_US(2);
GPIO_writePin(42, 0);
Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP3);
}

Thanks
Damien