Part Number: TMS320F28377D
Other Parts Discussed in Thread: UNIFLASH
We have build a board based on TMS320F28377D.
I could program once the internal Flash with Code Composer Studio, but could not erase/reprogramme it!
I can read memory content with UniFlash and a XDS2xx USB debug probe, but when I try to write or erase the internal Flash I've got following error messages:
[INFO] C28xx_CPU1: GEL Output: Memory Map Initialization Complete [ERROR] C28xx_CPU1: Error initializing flash programming: Interface returned from dll, but flash is not available on this device. [INFO] C28xx_CPU2: GEL Output: Memory Map Initialization Complete [ERROR] C28xx_CPU2: Error initializing flash programming: Interface returned from dll, but flash is not available on this device.
What is going wrong here?
Best regards
Fabrice Mousset