This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F28M35H52C: Programming issue

Part Number: F28M35H52C

Hi all,

I’ve a problem programming the microcontroller Concerto F28M35H52.

I have never had any problems in the past, but a few days ago I started having programming problems:

 

I was using XDS100v2 programmer, and at some point during the programming of the c28 core a program loading error appeared.

Trying again an error always appears but only for the C28 core, if I try to program the M3 core it programs correctly (also with another programmer XDS110).

Here the errors reported in the Console Window of CCS v.7:

Cortex_M3_0: GEL Output: Memory Map Initialization Complete
C28xx_0: GEL Output:
Memory Map Initialization Complete
C28xx_0: GEL Output:
RAM Initialization Complete
C28xx_0: Trouble Setting Breakpoint with the Action "Remain Halted" at 0x80e3: (Error -1066 @ 0x80E3) Unable to set/clear requested breakpoint. Verify that the breakpoint address is in valid memory. (Emulation package 6.0.579.0)
C28xx_0: Breakpoint Manager: Retrying with a AET breakpoint
C28xx_0: Can't Run Target CPU: (Error -1156 @ 0x8050) Device may be operating in low-power mode. Do you want to bring it out of this mode? Choose 'Yes' to force the device to wake up and retry the operation. Choose 'No' to retry the operation without waking the device. (Emulation package 6.0.579.0)
C28xx_0: Trouble Halting Target CPU: (Error -1135 @ 0x8050) The debug probe reported an error. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation. (Emulation package 6.0.579.0)
C28xx_0: Error: (Error -1135 @ 0x8050) The debug probe reported an error. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation. (Emulation package 6.0.579.0)
C28xx_0: Unable to determine target status after 20 attempts
C28xx_0: Failed to remove the debug state from the target before disconnecting. There may still be breakpoint op-codes embedded in program memory. It is recommended that you reset the emulator before you connect and reload your program before you continue debugging
C28xx_0: Error occurred during flash operation: Cannot disable hardware breakpoint while the target is halted. Halt the target and try again
C28xx_0: Error occurred during flash operation: Could not write 0x00000064@Data: target is not connected
C28xx_0: Error occurred during flash operation: Could not read 0x00004400@Data: target is not connected
C28xx_0: Error occurred during flash operation: Could not read 0x00004402@Data: target is not connected
C28xx_0: Error occurred during flash operation: Could not read 0x00004406@Data: target is not connected
C28xx_0: Error occurred during flash operation: Could not write 0x00000@Program: target is not connected
C28xx_0: Error occurred during flash operation: Cannot enable while the target is disconnected
C28xx_0: Error occurred during flash operation: Could not read 0x00000064@Data: target is not connected
C28xx_0: Error occurred during flash operation: Could not write 0x00000064@Data: target is not connected
C28xx_0: Error occurred during flash operation: Failed to run target while trying to execute pwrite_dis.alg
C28xx_0: Flash operation timed out waiting for the algorithm to complete. Operation cancelled.
C28xx_0: Error occurred during flash operation: Could not write 0x00000064@Data: target is not connected
C28xx_0: Error occurred during flash operation: Could not write 0x00004E26@Data: target is not connected
C28xx_0: Error occurred during flash operation: Could not read 0x04E26@Program: target is not connected
C28xx_0: Flash Programmer: Unable to acquire the clock semaphore. The other core might still be accessing the clock registers. Operation Cancelled.
C28xx_0: File Loader: Memory write failed: Unknown error
C28xx_0: GEL: File: D:\Firmware\1795_P1\C28\Release\C28.out: Load failed.
C28xx_0: Error occurred during flash operation: Could not read register PC: target is not connected
C28xx_0: Error occurred during flash operation: Could not write 0x00004000@Data: target is not connected
C28xx_0: Error occurred during flash operation: Could not write 0x00000@Program: target is not connected
C28xx_0: Error occurred during flash operation: Cannot enable while the target is disconnected
C28xx_0: Error occurred during flash operation: Could not read 0x00000064@Data: target is not connected
C28xx_0: Error occurred during flash operation: Could not write 0x00000064@Data: target is not connected
C28xx_0: Error occurred during flash operation: Failed to run target while trying to execute pwrite_en.alg
C28xx_0: Flash operation timed out waiting for the algorithm to complete. Operation cancelled.
C28xx_0: Error occurred during flash operation: Could not write 0x00000064@Data: target is not connected
C28xx_0: Error occurred during flash operation: Could not write 0x00004E26@Data: target is not connected
C28xx_0: Error occurred during flash operation: Could not read 0x04E26@Program: target is not connected
C28xx_0: Flash Programmer: Unable to acquire the clock semaphore. The other core might still be accessing the clock registers. Operation Cancelled.
C28xx_0: Error occurred during flash operation: Could not write register PC: target is not connected

I think the XDS100v2 programmer may have some problems and somehow corrupted the C28 core.

Is there any possibility of recovering the microcontroller or do I need to replace it with a new one?