Hello,
i have downloaded the CCS project of the reference design TI-02000 (Peak Current Mode Controlled PSFB Converter Reference Design Using C2000 Real-time MCU).
When i import the project in CCS the file "main.syscfg" doesn't open the GUI, and as result i cannot build the project. In the screenshot is visible the error tab.
The following TI software are installed on my machine:
-CCS Version: 11.2.0.00007
-C2000Ware 4_02_00_00
-C2000Ware 4_02_00_00
The operating system i'm using is Windows 7 Professional 64-bit SP1.
Thanks and kind regards,
Lorenzo