Other Parts Discussed in Thread: CONTROLSUITE
I see that in ControlSuite, there is a resolver library. It did not make it into the Motor Control SDK.
Are there any issues with compatibility, etc., if I would use the library with (a modified version of) a sample application from the Motor Control SDK (such as the Universal Motor Control lab)?
Are there other libraries, examples, etc. that I should look at for using a resolver with the Motor Control SDK?
Or does anyone otherwise have comments/tips for working with the resolver in the Motor Control SDK? (Such as in the control flow, where do I use the resolver library output?)
Thanks!
--Mark