Part Number: TMS320F28335
Hi, support team
My customer can not post on forum. I help him to ask a question:
TMS320F28335 Error(s) encountered while building model : ### Failed to generate all binary outputs
Could you give me a help?
The following is the complete code during building of program:
### Invoking Target Language Compiler on testadcsignal_MRAShard_15102022.rtw
### Using System Target File: C:\Program Files\MATLAB\MATLAB Production Server\R2015a\rtw\c\ert\ert.tlc
### Loading TLC function libraries
Warning: The data type "int8" uses a word size that is not available on the intended target.
Fixed-point signals using this data type will be put inside a larger word or multi words. When used,
extra software will be generated to force this larger word or multi words to emulate a smaller
word. This emulation is helpful when your prototype target and your final
production target are not the same. If the smaller word size does NOT exist
on the final production target, then consider increasing the word size to
one that is supported.
Warning: The data type "uint8" uses a word size that is not available on the intended target.
.
Warning: The data type "boolean" uses a word size that is not available on the intended target.
### Initial pass through model to cache user defined code
### Caching model source code
...............................................................................
...............................
### Writing source file testadcsignal_MRAShard_15102022.c
.
### Writing header file testadcsignal_MRAShard_15102022_private.h
### Writing header file testadcsignal_MRAShard_15102022.h
### Writing header file testadcsignal_MRAShard_15102022_types.h
### Writing header file rtwtypes.h
### Writing header file multiword_types.h
.
### Writing header file rt_nonfinite.h
### Writing source file rt_nonfinite.c
### Writing header file rtGetInf.h
### Writing source file rtGetInf.c
### Writing header file rtGetNaN.h
.
### Writing source file rtGetNaN.c
### Writing source file testadcsignal_MRAShard_15102022_data.c
### Writing header file rtmodel.h
### Writing source file ert_main.c
### TLC code generation complete.
### Generating TLC interface API.
...............................................................................
...........................................
### Creating data type transition file testadcsignal_MRAShard_15102022_dt.h
.### Evaluating PostCodeGenCommand specified in the model
### Using toolchain: Texas Instruments C2000 Code Generation Tools v5.2.12 | gmake (64-bit Windows)
### Creating 'C:\Rahul Singh_HM PC\MATLAB\testadcsignal_MRAShard_15102022_ert_rtw\testadcsignal_MRAShard_15102022.mk target="_blank">15102022.mk target="_blank">15102022.mk target="_blank">15102022.mk target="_blank">15102022.mk' ...
### Using toolchain: Texas Instruments C2000 Code Generation Tools v5.2.12 | gmake (64-bit Windows)
### Creating 'C:\Rahul Singh_HM PC\MATLAB\testadcsignal_MRAShard_15102022_ert_rtw\testadcsignal_MRAShard_15102022.mk' ...
### Building 'testadcsignal_MRAShard_15102022': C:\PROGRA~1\MATLAB\MATLAB~1\R2015a\bin\win64\gmake -B -f testadcsignal_MRAShard_15102022.mk all
C:\Rahul Singh_HM PC\MATLAB\testadcsignal_MRAShard_15102022_ert_rtw>cd .
C:\Rahul Singh_HM PC\MATLAB\testadcsignal_MRAShard_15102022_ert_rtw>if "" == "" (C:\PROGRA~1\MATLAB\MATLAB~1\R2015a\bin\win64\gmake -B -f testadcsignal_MRAShard_15102022.mk all ) else (C:\PROGRA~1\MATLAB\MATLAB~1\R2015a\bin\win64\gmake -B -f testadcsignal_MRAShard_15102022.mk )
C:/ti/ccsv5/tools/compiler/C2000_~1.0/bin/cl2000 --compile_only --large_memory_model --cla_support=cla0 --silicon_version=28 --define="LARGE_MODEL" -i"/~SupportFiles/DSP280x_headers" -i"/~SupportFiles/DSP280x_headers/include" -i"C:/ti/ccsv5/tools/compiler/C2000_~1.0/include" -v28 --float_support=fpu32 -ml --define="EXTMODE_DISABLEPRINTF" -v28 --float_support=fpu32 -ml -DMODEL=testadcsignal_MRAShard_15102022 -DNUMST=2 -DNCSTATES=0 -DHAVESTDIO -DON_TARGET_WAIT_FOR_START=0 -DONESTEPFCN=1 -DEXT_MODE=1 -DTERMFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=1 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DSTACK_SIZE=512 -DONESTEPFCN=1 -DEXT_MODE=1 -DTERMFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=1 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DON_TARGET_WAIT_FOR_START=0 -DRT -DSTACK_SIZE=512 -DMODEL=testadcsignal_MRAShard_15102022 -DNUMST=2 -DNCSTATES=0 -DHAVESTDIO -IC:/RAHULS~1/MATLAB/testadcsignal_MRAShard_15102022_ert_rtw -IC:/RAHULS~1/MATLAB -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/extern/include -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/simulink/include -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/rtw/c/src -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/rtw/c/src/ext_mode/common -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/rtw/c/ert -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/toolbox/coder/rtiostream/src/utils -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/toolbox/vision/include -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/toolbox/shared/dsp/vision/matlab/include -IC:/MATLAB/SupportPackages/R2015a/texasinstrumentsc2000/toolbox/target/supportpackages/tic2000/inc -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/toolbox/shared/can/src/scanutil -IC:/MATLAB/SupportPackages/R2015a/texasinstrumentsc2000/toolbox/target/supportpackages/tic2000/src -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/toolbox/target/extensions/processor/tic2000/include -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/toolbox/rtw/targets/common/can/blocks/tlc_c --output_file="MW_c28xx_board.obj" "C:/RAHULS~1/MATLAB/testadcsignal_MRAShard_15102022_ert_rtw/MW_c28xx_board.c"
C:/ti/ccsv5/tools/compiler/C2000_~1.0/bin/cl2000 --compile_only --large_memory_model --cla_support=cla0 --silicon_version=28 --define="LARGE_MODEL" -i"/~SupportFiles/DSP280x_headers" -i"/~SupportFiles/DSP280x_headers/include" -i"C:/ti/ccsv5/tools/compiler/C2000_~1.0/include" -v28 --float_support=fpu32 -ml --define="EXTMODE_DISABLEPRINTF" -v28 --float_support=fpu32 -ml -DMODEL=testadcsignal_MRAShard_15102022 -DNUMST=2 -DNCSTATES=0 -DHAVESTDIO -DON_TARGET_WAIT_FOR_START=0 -DONESTEPFCN=1 -DEXT_MODE=1 -DTERMFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=1 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DSTACK_SIZE=512 -DONESTEPFCN=1 -DEXT_MODE=1 -DTERMFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=1 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DON_TARGET_WAIT_FOR_START=0 -DRT -DSTACK_SIZE=512 -DMODEL=testadcsignal_MRAShard_15102022 -DNUMST=2 -DNCSTATES=0 -DHAVESTDIO -IC:/RAHULS~1/MATLAB/testadcsignal_MRAShard_15102022_ert_rtw -IC:/RAHULS~1/MATLAB -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/extern/include -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/simulink/include -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/rtw/c/src -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/rtw/c/src/ext_mode/common -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/rtw/c/ert -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/toolbox/coder/rtiostream/src/utils -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/toolbox/vision/include -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/toolbox/shared/dsp/vision/matlab/include -IC:/MATLAB/SupportPackages/R2015a/texasinstrumentsc2000/toolbox/target/supportpackages/tic2000/inc -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/toolbox/shared/can/src/scanutil -IC:/MATLAB/SupportPackages/R2015a/texasinstrumentsc2000/toolbox/target/supportpackages/tic2000/src -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/toolbox/target/extensions/processor/tic2000/include -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/toolbox/rtw/targets/common/can/blocks/tlc_c --output_file="MW_c28xx_adc.obj" "C:/RAHULS~1/MATLAB/testadcsignal_MRAShard_15102022_ert_rtw/MW_c28xx_adc.c"
C:/ti/ccsv5/tools/compiler/C2000_~1.0/bin/cl2000 --compile_only --large_memory_model --cla_support=cla0 --silicon_version=28 --define="LARGE_MODEL" -i"/~SupportFiles/DSP280x_headers" -i"/~SupportFiles/DSP280x_headers/include" -i"C:/ti/ccsv5/tools/compiler/C2000_~1.0/include" -v28 --float_support=fpu32 -ml --define="EXTMODE_DISABLEPRINTF" -v28 --float_support=fpu32 -ml -DMODEL=testadcsignal_MRAShard_15102022 -DNUMST=2 -DNCSTATES=0 -DHAVESTDIO -DON_TARGET_WAIT_FOR_START=0 -DONESTEPFCN=1 -DEXT_MODE=1 -DTERMFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=1 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DSTACK_SIZE=512 -DONESTEPFCN=1 -DEXT_MODE=1 -DTERMFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=1 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DON_TARGET_WAIT_FOR_START=0 -DRT -DSTACK_SIZE=512 -DMODEL=testadcsignal_MRAShard_15102022 -DNUMST=2 -DNCSTATES=0 -DHAVESTDIO -IC:/RAHULS~1/MATLAB/testadcsignal_MRAShard_15102022_ert_rtw -IC:/RAHULS~1/MATLAB -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/extern/include -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/simulink/include -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/rtw/c/src -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/rtw/c/src/ext_mode/common -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/rtw/c/ert -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/toolbox/coder/rtiostream/src/utils -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/toolbox/vision/include -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/toolbox/shared/dsp/vision/matlab/include -IC:/MATLAB/SupportPackages/R2015a/texasinstrumentsc2000/toolbox/target/supportpackages/tic2000/inc -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/toolbox/shared/can/src/scanutil -IC:/MATLAB/SupportPackages/R2015a/texasinstrumentsc2000/toolbox/target/supportpackages/tic2000/src -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/toolbox/target/extensions/processor/tic2000/include -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/toolbox/rtw/targets/common/can/blocks/tlc_c --output_file="MW_c28xx_csl.obj" "C:/RAHULS~1/MATLAB/testadcsignal_MRAShard_15102022_ert_rtw/MW_c28xx_csl.c"
C:/ti/ccsv5/tools/compiler/C2000_~1.0/bin/cl2000 --compile_only --large_memory_model --cla_support=cla0 --silicon_version=28 --define="LARGE_MODEL" -i"/~SupportFiles/DSP280x_headers" -i"/~SupportFiles/DSP280x_headers/include" -i"C:/ti/ccsv5/tools/compiler/C2000_~1.0/include" -v28 --float_support=fpu32 -ml --define="EXTMODE_DISABLEPRINTF" -v28 --float_support=fpu32 -ml -DMODEL=testadcsignal_MRAShard_15102022 -DNUMST=2 -DNCSTATES=0 -DHAVESTDIO -DON_TARGET_WAIT_FOR_START=0 -DONESTEPFCN=1 -DEXT_MODE=1 -DTERMFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=1 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DSTACK_SIZE=512 -DONESTEPFCN=1 -DEXT_MODE=1 -DTERMFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=1 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DON_TARGET_WAIT_FOR_START=0 -DRT -DSTACK_SIZE=512 -DMODEL=testadcsignal_MRAShard_15102022 -DNUMST=2 -DNCSTATES=0 -DHAVESTDIO -IC:/RAHULS~1/MATLAB/testadcsignal_MRAShard_15102022_ert_rtw -IC:/RAHULS~1/MATLAB -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/extern/include -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/simulink/include -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/rtw/c/src -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/rtw/c/src/ext_mode/common -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/rtw/c/ert -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/toolbox/coder/rtiostream/src/utils -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/toolbox/vision/include -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/toolbox/shared/dsp/vision/matlab/include -IC:/MATLAB/SupportPackages/R2015a/texasinstrumentsc2000/toolbox/target/supportpackages/tic2000/inc -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/toolbox/shared/can/src/scanutil -IC:/MATLAB/SupportPackages/R2015a/texasinstrumentsc2000/toolbox/target/supportpackages/tic2000/src -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/toolbox/target/extensions/processor/tic2000/include -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/toolbox/rtw/targets/common/can/blocks/tlc_c --output_file="MW_c28xx_pwm.obj" "C:/RAHULS~1/MATLAB/testadcsignal_MRAShard_15102022_ert_rtw/MW_c28xx_pwm.c"
C:/ti/ccsv5/tools/compiler/C2000_~1.0/bin/cl2000 --compile_only --large_memory_model --cla_support=cla0 --silicon_version=28 --define="LARGE_MODEL" -i"/~SupportFiles/DSP280x_headers" -i"/~SupportFiles/DSP280x_headers/include" -i"C:/ti/ccsv5/tools/compiler/C2000_~1.0/include" -v28 --float_support=fpu32 -ml --define="EXTMODE_DISABLEPRINTF" -v28 --float_support=fpu32 -ml -DMODEL=testadcsignal_MRAShard_15102022 -DNUMST=2 -DNCSTATES=0 -DHAVESTDIO -DON_TARGET_WAIT_FOR_START=0 -DONESTEPFCN=1 -DEXT_MODE=1 -DTERMFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=1 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DSTACK_SIZE=512 -DONESTEPFCN=1 -DEXT_MODE=1 -DTERMFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=1 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DON_TARGET_WAIT_FOR_START=0 -DRT -DSTACK_SIZE=512 -DMODEL=testadcsignal_MRAShard_15102022 -DNUMST=2 -DNCSTATES=0 -DHAVESTDIO -IC:/RAHULS~1/MATLAB/testadcsignal_MRAShard_15102022_ert_rtw -IC:/RAHULS~1/MATLAB -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/extern/include -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/simulink/include -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/rtw/c/src -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/rtw/c/src/ext_mode/common -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/rtw/c/ert -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/toolbox/coder/rtiostream/src/utils -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/toolbox/vision/include -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/toolbox/shared/dsp/vision/matlab/include -IC:/MATLAB/SupportPackages/R2015a/texasinstrumentsc2000/toolbox/target/supportpackages/tic2000/inc -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/toolbox/shared/can/src/scanutil -IC:/MATLAB/SupportPackages/R2015a/texasinstrumentsc2000/toolbox/target/supportpackages/tic2000/src -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/toolbox/target/extensions/processor/tic2000/include -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/toolbox/rtw/targets/common/can/blocks/tlc_c --output_file="MW_c28xx_qep.obj" "C:/RAHULS~1/MATLAB/testadcsignal_MRAShard_15102022_ert_rtw/MW_c28xx_qep.c"
C:/ti/ccsv5/tools/compiler/C2000_~1.0/bin/cl2000 --compile_only --large_memory_model --cla_support=cla0 --silicon_version=28 --define="LARGE_MODEL" -i"/~SupportFiles/DSP280x_headers" -i"/~SupportFiles/DSP280x_headers/include" -i"C:/ti/ccsv5/tools/compiler/C2000_~1.0/include" -v28 --float_support=fpu32 -ml --define="EXTMODE_DISABLEPRINTF" -v28 --float_support=fpu32 -ml -DMODEL=testadcsignal_MRAShard_15102022 -DNUMST=2 -DNCSTATES=0 -DHAVESTDIO -DON_TARGET_WAIT_FOR_START=0 -DONESTEPFCN=1 -DEXT_MODE=1 -DTERMFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=1 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DSTACK_SIZE=512 -DONESTEPFCN=1 -DEXT_MODE=1 -DTERMFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=1 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DON_TARGET_WAIT_FOR_START=0 -DRT -DSTACK_SIZE=512 -DMODEL=testadcsignal_MRAShard_15102022 -DNUMST=2 -DNCSTATES=0 -DHAVESTDIO -IC:/RAHULS~1/MATLAB/testadcsignal_MRAShard_15102022_ert_rtw -IC:/RAHULS~1/MATLAB -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/extern/include -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/simulink/include -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/rtw/c/src -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/rtw/c/src/ext_mode/common -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/rtw/c/ert -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/toolbox/coder/rtiostream/src/utils -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/toolbox/vision/include -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/toolbox/shared/dsp/vision/matlab/include -IC:/MATLAB/SupportPackages/R2015a/texasinstrumentsc2000/toolbox/target/supportpackages/tic2000/inc -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/toolbox/shared/can/src/scanutil -IC:/MATLAB/SupportPackages/R2015a/texasinstrumentsc2000/toolbox/target/supportpackages/tic2000/src -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/toolbox/target/extensions/processor/tic2000/include -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/toolbox/rtw/targets/common/can/blocks/tlc_c --output_file="rtGetInf.obj" "C:/RAHULS~1/MATLAB/testadcsignal_MRAShard_15102022_ert_rtw/rtGetInf.c"
C:/ti/ccsv5/tools/compiler/C2000_~1.0/bin/cl2000 --compile_only --large_memory_model --cla_support=cla0 --silicon_version=28 --define="LARGE_MODEL" -i"/~SupportFiles/DSP280x_headers" -i"/~SupportFiles/DSP280x_headers/include" -i"C:/ti/ccsv5/tools/compiler/C2000_~1.0/include" -v28 --float_support=fpu32 -ml --define="EXTMODE_DISABLEPRINTF" -v28 --float_support=fpu32 -ml -DMODEL=testadcsignal_MRAShard_15102022 -DNUMST=2 -DNCSTATES=0 -DHAVESTDIO -DON_TARGET_WAIT_FOR_START=0 -DONESTEPFCN=1 -DEXT_MODE=1 -DTERMFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=1 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DSTACK_SIZE=512 -DONESTEPFCN=1 -DEXT_MODE=1 -DTERMFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=1 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DON_TARGET_WAIT_FOR_START=0 -DRT -DSTACK_SIZE=512 -DMODEL=testadcsignal_MRAShard_15102022 -DNUMST=2 -DNCSTATES=0 -DHAVESTDIO -IC:/RAHULS~1/MATLAB/testadcsignal_MRAShard_15102022_ert_rtw -IC:/RAHULS~1/MATLAB -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/extern/include -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/simulink/include -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/rtw/c/src -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/rtw/c/src/ext_mode/common -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/rtw/c/ert -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/toolbox/coder/rtiostream/src/utils -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/toolbox/vision/include -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/toolbox/shared/dsp/vision/matlab/include -IC:/MATLAB/SupportPackages/R2015a/texasinstrumentsc2000/toolbox/target/supportpackages/tic2000/inc -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/toolbox/shared/can/src/scanutil -IC:/MATLAB/SupportPackages/R2015a/texasinstrumentsc2000/toolbox/target/supportpackages/tic2000/src -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/toolbox/target/extensions/processor/tic2000/include -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/toolbox/rtw/targets/common/can/blocks/tlc_c --output_file="rtGetNaN.obj" "C:/RAHULS~1/MATLAB/testadcsignal_MRAShard_15102022_ert_rtw/rtGetNaN.c"
C:/ti/ccsv5/tools/compiler/C2000_~1.0/bin/cl2000 --compile_only --large_memory_model --cla_support=cla0 --silicon_version=28 --define="LARGE_MODEL" -i"/~SupportFiles/DSP280x_headers" -i"/~SupportFiles/DSP280x_headers/include" -i"C:/ti/ccsv5/tools/compiler/C2000_~1.0/include" -v28 --float_support=fpu32 -ml --define="EXTMODE_DISABLEPRINTF" -v28 --float_support=fpu32 -ml -DMODEL=testadcsignal_MRAShard_15102022 -DNUMST=2 -DNCSTATES=0 -DHAVESTDIO -DON_TARGET_WAIT_FOR_START=0 -DONESTEPFCN=1 -DEXT_MODE=1 -DTERMFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=1 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DSTACK_SIZE=512 -DONESTEPFCN=1 -DEXT_MODE=1 -DTERMFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=1 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DON_TARGET_WAIT_FOR_START=0 -DRT -DSTACK_SIZE=512 -DMODEL=testadcsignal_MRAShard_15102022 -DNUMST=2 -DNCSTATES=0 -DHAVESTDIO -IC:/RAHULS~1/MATLAB/testadcsignal_MRAShard_15102022_ert_rtw -IC:/RAHULS~1/MATLAB -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/extern/include -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/simulink/include -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/rtw/c/src -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/rtw/c/src/ext_mode/common -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/rtw/c/ert -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/toolbox/coder/rtiostream/src/utils -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/toolbox/vision/include -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/toolbox/shared/dsp/vision/matlab/include -IC:/MATLAB/SupportPackages/R2015a/texasinstrumentsc2000/toolbox/target/supportpackages/tic2000/inc -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/toolbox/shared/can/src/scanutil -IC:/MATLAB/SupportPackages/R2015a/texasinstrumentsc2000/toolbox/target/supportpackages/tic2000/src -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/toolbox/target/extensions/processor/tic2000/include -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/toolbox/rtw/targets/common/can/blocks/tlc_c --output_file="rt_nonfinite.obj" "C:/RAHULS~1/MATLAB/testadcsignal_MRAShard_15102022_ert_rtw/rt_nonfinite.c"
C:/ti/ccsv5/tools/compiler/C2000_~1.0/bin/cl2000 --compile_only --large_memory_model --cla_support=cla0 --silicon_version=28 --define="LARGE_MODEL" -i"/~SupportFiles/DSP280x_headers" -i"/~SupportFiles/DSP280x_headers/include" -i"C:/ti/ccsv5/tools/compiler/C2000_~1.0/include" -v28 --float_support=fpu32 -ml --define="EXTMODE_DISABLEPRINTF" -v28 --float_support=fpu32 -ml -DMODEL=testadcsignal_MRAShard_15102022 -DNUMST=2 -DNCSTATES=0 -DHAVESTDIO -DON_TARGET_WAIT_FOR_START=0 -DONESTEPFCN=1 -DEXT_MODE=1 -DTERMFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=1 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DSTACK_SIZE=512 -DONESTEPFCN=1 -DEXT_MODE=1 -DTERMFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=1 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DON_TARGET_WAIT_FOR_START=0 -DRT -DSTACK_SIZE=512 -DMODEL=testadcsignal_MRAShard_15102022 -DNUMST=2 -DNCSTATES=0 -DHAVESTDIO -IC:/RAHULS~1/MATLAB/testadcsignal_MRAShard_15102022_ert_rtw -IC:/RAHULS~1/MATLAB -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/extern/include -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/simulink/include -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/rtw/c/src -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/rtw/c/src/ext_mode/common -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/rtw/c/ert -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/toolbox/coder/rtiostream/src/utils -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/toolbox/vision/include -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/toolbox/shared/dsp/vision/matlab/include -IC:/MATLAB/SupportPackages/R2015a/texasinstrumentsc2000/toolbox/target/supportpackages/tic2000/inc -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/toolbox/shared/can/src/scanutil -IC:/MATLAB/SupportPackages/R2015a/texasinstrumentsc2000/toolbox/target/supportpackages/tic2000/src -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/toolbox/target/extensions/processor/tic2000/include -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/toolbox/rtw/targets/common/can/blocks/tlc_c --output_file="testadcsignal_MRAShard_15102022.obj" "C:/RAHULS~1/MATLAB/testadcsignal_MRAShard_15102022_ert_rtw/testadcsignal_MRAShard_15102022.c"
"C:\Users\Vinod\AppData\Local\Temp\0168410", ERROR! at line 6682:
[E5369]
Due to FPU pipeline restriction, this instruction is illegal in the 5
delay slots of: [MOV32 R0H,ACC ; [CPU_] |1400|,
line 6678]
F32TOUI32 R0H,R0H ; [CPU_] |1400|
"C:\Users\Vinod\AppData\Local\Temp\0168410", ERROR! at line 6751:
[E5369]
Due to FPU pipeline restriction, this instruction is illegal in the 5
delay slots of: [MOV32 R0H,ACC ; [CPU_] |1415|,
line 6747]
F32TOUI32 R0H,R0H ; [CPU_] |1415|
"C:\Users\Vinod\AppData\Local\Temp\0168410", ERROR! at line 6895:
[E5369]
Due to FPU pipeline restriction, this instruction is illegal in the 5
delay slots of: [MOV32 R0H,ACC ; [CPU_] |1461|,
line 6891]
F32TOUI32 R0H,R0H ; [CPU_] |1461|
"C:\Users\Vinod\AppData\Local\Temp\0168410", ERROR! at line 6956:
[E5369]
Due to FPU pipeline restriction, this instruction is illegal in the 5
delay slots of: [MOV32 R0H,ACC ; [CPU_] |1482|,
line 6952]
F32TOUI32 R0H,R0H ; [CPU_] |1482|
"C:\Users\Vinod\AppData\Local\Temp\0168410", ERROR! at line 7079:
[E5369]
Due to FPU pipeline restriction, this instruction is illegal in the 5
delay slots of: [MOV32 R0H,ACC ; [CPU_] |1521|,
line 7075]
F32TOUI32 R0H,R0H ; [CPU_] |1521|
"C:\Users\Vinod\AppData\Local\Temp\0168410", ERROR! at line 7140:
[E5369]
Due to FPU pipeline restriction, this instruction is illegal in the 5
delay slots of: [MOV32 R0H,ACC ; [CPU_] |1542|,
line 7136]
F32TOUI32 R0H,R0H ; [CPU_] |1542|
"C:\Users\Vinod\AppData\Local\Temp\0168410", ERROR! at line 8383:
[E5369]
Due to FPU pipeline restriction, this instruction is illegal in the 5
delay slots of: [MOV32 R0H,ACC ; [CPU_] |2284|,
line 8379]
F32TOUI32 R0H,R0H ; [CPU_] |2284|
"C:\Users\Vinod\AppData\Local\Temp\0168410", ERROR! at line 8452:
[E5369]
Due to FPU pipeline restriction, this instruction is illegal in the 5
delay slots of: [MOV32 R0H,ACC ; [CPU_] |2300|,
line 8448]
F32TOUI32 R0H,R0H ; [CPU_] |2300|
"C:\Users\Vinod\AppData\Local\Temp\0168410", ERROR! at line 8592:
[E5369]
Due to FPU pipeline restriction, this instruction is illegal in the 5
delay slots of: [MOV32 R0H,ACC ; [CPU_] |2354|,
line 8588]
F32TOUI32 R0H,R0H ; [CPU_] |2354|
"C:\Users\Vinod\AppData\Local\Temp\0168410", ERROR! at line 8715:
[E5369]
Due to FPU pipeline restriction, this instruction is illegal in the 5
delay slots of: [MOV32 R0H,ACC ; [CPU_] |2389|,
line 8711]
F32TOUI32 R0H,R0H ; [CPU_] |2389|
"C:\Users\Vinod\AppData\Local\Temp\0168410", ERROR! at line 8859:
[E5369]
Due to FPU pipeline restriction, this instruction is illegal in the 5
delay slots of: [MOV32 R0H,ACC ; [CPU_] |2448|,
line 8855]
F32TOUI32 R0H,R0H ; [CPU_] |2448|
"C:\Users\Vinod\AppData\Local\Temp\0168410", ERROR! at line 8928:
[E5369]
Due to FPU pipeline restriction, this instruction is illegal in the 5
delay slots of: [MOV32 R0H,ACC ; [CPU_] |2464|,
line 8924]
F32TOUI32 R0H,R0H ; [CPU_] |2464|
"C:\Users\Vinod\AppData\Local\Temp\0168410", ERROR! at line 8997:
[E5369]
Due to FPU pipeline restriction, this instruction is illegal in the 5
delay slots of: [MOV32 R0H,ACC ; [CPU_] |2478|,
line 8993]
F32TOUI32 R0H,R0H ; [CPU_] |2478|
13 Assembly Errors, No Assembly Warnings
Errors in Source - Assembler Aborted
>> Compilation failure
gmake: *** [testadcsignal_MRAShard_15102022.obj] Error 1
C:\Rahul Singh_HM PC\MATLAB\testadcsignal_MRAShard_15102022_ert_rtw>echo The make command returned an error of 2
The make command returned an error of 2
C:\Rahul Singh_HM PC\MATLAB\testadcsignal_MRAShard_15102022_ert_rtw>An_error_occurred_during_the_call_to_make
'An_error_occurred_during_the_call_to_make' is not recognized as an internal or external command,
operable program or batch file.
### Build procedure for model: 'testadcsignal_MRAShard_15102022' aborted due to an error.
Error(s) encountered while building model "testadcsignal_MRAShard_15102022":
### Failed to generate all binary outputs.
Component: Simulink | Category: Model error
Thanks so much.
Best regards,
Yuki