Part Number: DRV8301-69M-KIT
Hi Team,
Good day. I am posting this inquiry on behalf or the customer.
"I already purchased a 69m kit for foc control of a brushless dc motor, but I wonder with some modifications in the hardware of the MISO CONTROL CARD 28069x can I use each half-bridge separately and test in three single-phase AC loads or three dc loads (i mean that I can control the three half-bridge separately) or it would be difficult to do because that kit was designed to control DC, and PMSG motors? (asic ac motors can be controlled to, but the maximum output voltage by the kit was 50V and 3.5 amps in DC so almost no asic AC motor for that power rating)."
Please help to advise. Thank you for extending your help.
Kind regards,
Marvin