This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CAN boot for TMS320F28069M MCU

Other Parts Discussed in Thread: C2000WARE, TMS320F28069M

Hi,

I want to update the flash memory via CAN. According to the MCU document, it is mentioned that the OTP value should be changed to boot from CAN. Also pin configuration for CAN boot is not mentioned. So I have changed the OTP value for the GETMODE according to the Application note attached herewith. 

RESULT: -The MCU will not BOOT as default. Always the MCU is waiting for CAN data. Although the power reset, normal boot is not happening. Now it is not standalone working. Now I can upload codes only from the JTAG using debugger. 

QUESTION: - How to change the MCU to the default BOOT mode again without looking for CAN data again and again?

Hoping an immediate reply as soon as possible.