This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-F28027: LAUNCHXL-F28027

Part Number: LAUNCHXL-F28027
Other Parts Discussed in Thread: C2000WARE

Currently, I am working using the launch pad F28027 (C2000 Piccolo) kit. I am working with MATLAB for the firmware development , i am able to generate the code from the MATLAB but when i am trying to flash the  code into the microcontroller i am getting the below error.

Debug Server Scripting (DSS) error: SLF4J: Failed to load class "org.slf4j.impl.StaticLoggerBinder"

I tried to resolve this error but could not do so. please help with this error , i think this related to CCS. 

However, I have installed all the required coding packages (MATLAB, Simulink and Embedded Coder) which are required to run. I think it is an error that due to the CCS software.