Part Number: TMS320F280049C
I'm experiencing strange behavior related to breakpoints in CCS version 10.2.0.00009
See attached example
In this example I have a breakpoint set inside an if statement. I'm not expecting the breakpoint to be activated because the if should be evaluated as false, however the program does halt at the breakpoint.
As shown when I hover over keys, IN_MM has a value of 0.
Interestingly if I set the breakpoint at line 316 and then do a single step the program skips over this if statement entirely as I would expect it to.
I have re-compiled, re-saved, re-loaded etc. and regardless CCS halts unexpectedly at this line.
What's up with this or what am I doing incorrectly