This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28388D: difference between CLB and FPGA

Part Number: TMS320F28388D


Hi Team,

Here're some issues from the customer may need your help:

How many tiles does CLB need to collect encoder data?

What's the difference between CLB and FPGA? Like processing speed. 

Thanks & Regards

Yale Li

  • Hi Yale,

    The CLB-based encoder implementation only requires a single CLB tile to implement the decoding logic. You can find more information about that within the PTO API reference guide at: http://ti.com/lit/sprac77

    There are some major differences between the CLB and FPGA, I would recommend looking at the C2000 Academy CLB Module for a basic understanding of it. In terms of the differences between the two, the CLB is of course more limited in terms of resources and is not as feature-packed as an FPGA. However, depending on what is needing to be implemented, the CLB can be more than enough. In terms of processing speed, the CLB on the F28388D is running at 100 MHz or 150 MHz in pipeline mode. The processing speed on an FPGA is dependent on the FPGA and how you are transferring information between the two devices. I would say that the CLB is beneficial in that it is already clocked with the device which is a huge advantage. 

    Please let me know if this answered your question or if you have any other specific inquiries about the CLB

    Regards,

    Peter